Argentinian Brutus At Work | Cummins Inc.
""
Marine

Argentinian Brutus At Work

by Alan Haig-Brown

Cummins Vessel Reference #789

 

 

The Brutus alongside for commissioning ceremonies.

 

In May of 2016 the Argentinian-designed and built 28.77 by 10.2-meter ASD tug Brutus went to work in the Harbor at Buenos Aries. This marked a milestone in Argentinian maritime affairs, as it is, at 5,400 HP, the most powerful ship-handling tug in the country.


 

A pair of Cummins QSK60 engines deliver 5400 HP and a 75-ton bollard pull.

 

The tug was designed by Ing. Emilio Noël and built by Unidelta Shipyards S.A., which has a well-established reputation in a wide range of steel and aluminum workboats. The yard has a plant located in Buenos Aires with 10,000 cubic meters of open and 4,000 cu.m. of covered work space. The shipyard also has an engineering office located in the City of Buenos Aires.

 

 

Brutus will work ships over the bow….

 

 

The new tug has joined a fleet of pilot boats and tugs owned by the SIP Pilotale & Practicaje, a firm providing pilotage in the Port of Buenos Aires and on the Rio de la Plata. The firm also has a Research and Training Maritime Center providing a wide range of trainings including the use of a simulator. (http://www.sipsa.com.ar)

 

 

 

and tow barges over the stern.

 

The vessel’s 4.7 meter depth includes the two Rolls-Royce Azimuthing Thrusters, Type US 205/P20 FP. Each of these aft-mounted thrusters is powered by a 16-cylinder Cummins QSK60M diesel engine generating 2700 HP (2013 kW) at 1900 RPM.

 

 

With good visibility both fore and aft.

 

With a design speed of 12-knots the 5400 HP tug delivers 75-tons of bollard pull. On the fore deck a combination Rolls-Royce Hydraulic Towing and anchor winch has been installed. On the aft deck, is a Mapawey Quick Release Disc-type Towing hook, Type DCX50/65 with a 65-ton load release. Other aft-deck equipment includes a three-ton capstan.

 

The tug is also fitted with a diesel driven pump-set powered by a Cummins 6BT5.9-D(M) capable of delivering 200 cubic-meters per hour to two monitors each capable of 100 cu.m. per hour. Two 80 kW gensets are each powered by a Cummins 6B-CP engine.

Accommodation is provided for up to ten crewmembers. Tankage includes 107.4 cubic-meters of fuel, 15.8 cu.mt. of water and 6.5 cu.mt. of lube oil. The vessel is certified Lloyd’s Register Class Notation ?100A1 tug / Remolcador de Tiro de navegación Marítima Nacional, Prefectura Naval Argentina.

 

Photos and video of the Brutus are courtesy of Cummins Argentina

 

www.youtube.com/watch?v=eyH2T8bl2C8&feature=youtu.be

 

For further information:

 

Boat Builder:
Astilleros Uni delta S. A.
Chubut 1350, 1624 Rincón de Milberg,
Buenos Aires, Argentina
Phone: 54 11 4749 9112

Boat Designer:
Ing. Emilio Noël
San Martín 981, Piso 4, Oficina 14, 1004 CABA,
Argentina
Phone: 54 11 4311 7782

Engine supply:
Armando Tavarozzi
HHP Sales Engines Leader
Cummins Distribution
Ruta Panamericana Km. 32,5
El Talar, Buenos Aires, Argentina
Tel: 54 11 4736-6428
Phone: 54 11 3280-8713
E-mail: [email protected]
 

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...