Hybrid Electrical Service for Stern Trawler | Cummins Inc.
Ship at sea
Marine

Hybrid Electrical Service for Stern Trawler

by Alan Haig-Brown

Fish companies from New Zealand to Russia (currently 24 large and ultra large Russian vessels) and Iceland to the USA as well as Greenland and now Canada have chosen the Norwegian firm Skipsteknisk when it comes time to design a new vessel. The firm has garnered a reputation for designing and overseeing the construction of vessels that integrate the most up to date technology from deck equipment to processing and stowage.

Stern Trawler

Ocean Choice International, of St. Johns, Newfoundland, Canada has ordered a new 74 by16-meter freezer trawler to be built at the Tersan Shipyard in Turkey. For the design work, both hull and equipment, they went to Skipsteknisk. Given the vessel size and freezing capacity, electrical generation is an important consideration in the design.

Stern Trawler4

In addition to a6528-hp MAN main engine the naval architects designed in a Cummins QSK 60-powered generator with an output of 2155KVA/ 1724KWe, 3x440VAC, 3 phase, 60hz. An additional Cummins QSK19-powered generator has an output of 700 KVA / 560KWe, 3x440VAC, 3 phase, 60 Hz.

These will meet the extensive electrical needs of the vessel’s 39-crew accommodation block, extensive navigation suite, and processing factory. Most importantly the large freezer capacity will have a significant draw.

Stern Trawler 3

It is to partially meet electrical demands of the trawler that Ibercisa electric winches have been selected. These trawl winches have a remarkable quality, when the net is being payed out, the force of the turning winch generated electricity. It is similar to a hybrid car going down hill, but the new energy is not stored in a battery.

Inge Bertil Straume of Skipsteknisk explains, “By the use of active front end (AFE) technology, we are able to utilize regenerative power from the winches when paying out the trawl gear. Thus the winches work as a “power plant”.
“This free power will normally be utilized through the other major consumers on-board, like fish-factory, freezing machinery and the hotel load. In the case of low demand on-board, this free power will be put on the propeller through the gearbox shaft alternator / motor ( in PTI mode).”

Of course the power from the winch is intermittent and small compared to the demands of the vessel. The electric winches make heavy demand when the gear is being retrieved. The two Cummins-powered, IMO 3 certified, generator sets will meet the vessel’s extensive electrical requirements.

Delivery of the, as yet unnamed, vessel is scheduled for the fourth quarter of 2019.

For further information:
Inge Bertil Straume

Sales Manager Fishing Vessels
Skipsteknisk AS

Klaus Nilsens gt. 4, P.O.Box 36 Sentrum, NO-6001 
Aalesund, Norway, 
E-mail: [email protected]
Phone: +47 70 10 33 44, Direct: +47 70 10 33 70
Mobile: +47 91 66 00 11 Fax: +47 70 10 33 48
www.skipsteknisk.no

Elshad Asadi
Cummins Marine Sales
Istanbul, Turkey
E-mail: [email protected]

A. Haig-Brown Ltd.
www.haigbrown.com
[email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...