LPG Tanker for the Mekong River | Cummins Inc.
""
Marine

LPG Tanker for the Mekong River

by Alan Haig-Brown

Cummins Vessel Reference #719

The 1400 cubic meter capacity LPG tanker ready for delivery.

The Saigon Shipbuilding & Marine Industries One Member Co, Ltd. (Saigon Shipmarin) has completed construction of a 60 by 11-meter LPG carrier. With capacity for 1400 cubic meters in two tanks the vessel’s hull has a 4-meter molded depth and a 2.6-meter draft.

Designed by a related company to Saigon Shipmarin, the vessel, to be named FACO, is owned by the F.A. Joint Stock Company. Being built to the Vietnam Register Rules and National Inland Regulations, the vessel will be classed for near shore and river operations. A pair of Cummins 855 diesels delivering 400 HP each provide propulsion power. Two Cumming 6C engines power 120 kW generator sets.

This is the first vessel built by the yard to this design but it is anticipated that this may well be the first of a growing class.

 


Saigon Shipmarin is a member of SBIC (Shipbuilding Industry Corporation) and is under the control of the Vietnam Ministry of Transport. The yard, located at Ho Chi Minh City, operates as a new building and ship repair facility. The yard’s products include OSVs, tugs boats, LPG tankers, and passenger vessels.


For more information:

Vu Cong Vuong
Sales Manager
Saigon Shipmarin
No. 2 – Dao Tri St. – Phu Thuan Ward
District 7 – Ho Chi Minh City
Phone: 84 8 37730 234 3381
Mobile: 84 8 0903 737 872
E-mail: [email protected]
Web: www.ssmi.com.vn

Vu Duc Tri
Business Development Manager
1st Floor, Etown 2 Building, 364 Cong Hoa Street,
Ward 13, Tan Binh District, Ho Chi Minh City
Vietnam
Phone: 84 8 38 134 124 | Extension: 719
Mobile: 84 933 064 306
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...