Towboats Still in Demand | Cummins Inc.
""
Marine

Towboats Still in Demand

by Alan Haig-Brown

Cummins Vessel Reference #610

The towboat Baffin Bay on the Tennessee River. Jeff L. Yates photo

In spite of the economic gloom of 2010, the demand for solid reliable towboats for the US Inland waterways has continued. An example of this is Higman Marine Services’ latest addition. The final month of 2010 saw yet another towboat added to the fleet of their subsidiary Higman Barge Lines. As with many earlier boats The M/V Baffin Bay was built by Hope Services of Dulac Louisiana. But this boat is one of the newly designed and larger 78 by 34-foot vessels. Hull number 174 from Hope’s yard is also the 36th vessel from Hope for Higman.

The boat continued the long established practice at Hope Services of installing a pair of 38-liter Cummins tier 2 compliant KTA38 engines each rated for 1000 HP at 1800 RPM. The engines turn into Twin Disc540 gears with 6.14:1 reduction. The two 85 kW generator sets are powered by Cummins 6BTA engines.

Paducah Kentucky-based photographer Jeff L. Yates took the attached photo ion January 7, 2011 as she was holding against the right descending bank of the Tennessee River, probably waiting for improved weather conditions on the Ohio River. Jeff reports that she was en-route from Decatur, Alabama to Houston Texas and pushing two barges at the time.


For further information:

Joe Gregory
Territory Sales Manager
Cummins Mid-South, Inc.
110 East Airline Hwy.
Kenner, LA 70062
USA
Phone: 504 465 3404
E-mail: [email protected]

Rocky Henderson
President
Hope Services Inc.
8506 Shrimpers Row,
Dulac, LA 70353-2206
Phone: 985 563 7801
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...