Versatile Response Vessel from Russia | Cummins Inc.
""
Marine

Versatile Response Vessel from Russia

by Alan Haig-Brown

Cummins Vessel Reference #790

The TG17 rendering shows a good looking and versatile boat.

 

A challenge for designers or an emergency response vessel is deciding to what type of emergency the boat will respond. The designers at the non-government Marine Engineering Bureau in Odessa Ukraine have fitted a very wide range of capabilities into their 31.73 by 9.7-meter tug. The vessel’s beams and 4.1-meter molded depth will give it the stability for handling heavy ships.

 

The azimuthing stern drive tug will be ready to handle a wide range of services. These will range from towing various objects to auxiliary operations in the harbour area. These latter will include oil spill response as auxiliary transport for equipment, installation of booms, assistance in fire fighting, loading and off loading of cargo with deck crane.

Power for this wide range of applications is to be supplied by a pair of Cummins K38-M main engines each delivering 634 kW to Z-drives. Auxiliary power will be provided by two Cummins NTA855-CP200DM5 generators sets each delivering 200 kW. The tug has two forward mounted fire monitors.

 

The after deck features a crane and a towing winch.

 

A towing winch with a 20-ton braking power, is mounted on the aft deck, as is a cargo crane. The crane can also serve to launch the rescue craft mounted atop the deckhouse.

 

The tug is being built to the Russian Maritime Register of Shipping class KM Arc 4 R1 AUT3-C FF3WS Tug. Currently under construction at the Okskaya Sudoverf “OKA” shipyard on the Oka River in Navashino, Russia, the boat is scheduled for delivery in 2016.

 

Renderings are courtesy of the Marine Engineering Bureau.

 

For further information:

 

Marine Engineering Bureau
15, Tenistaya str.,
Odessa, 65009, Ukraine
Phone: 380 482 347928 | 380 48 7480696 | 7149272
Fax: 380 482 356005
E-mail: [email protected]

 

Alexander Dunkov
Marine Sales Manager
Cummins Russia and CIS
Phone: 7 812 57007798
Mobile: 7 961 800 06 42 
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...