Case Studies | Cummins Inc.

Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

Overview Challenge: Red Cross Hospital in Cordoba, Spain needed to replace an older outdated backup genset with a new genset that provided 220 kva. In addition, the removal of the old genset and installation of the new backup genset needed to take place within a 24-hour period without leaving the hospital at risk during an outage. Solution: The

Overview Challenge: Design and install an emergency standby power system as part of a major upgrade at AnMed Medical Center in Anderson, SC Solution: Cummins installed three 2000 kW diesel fueled generator sets, transfer switches and digital master control (DMC). Prior to installation, a factory “witness” test was conducted at the Cummins plant

Overview Challenge: Krankenhaus Bozen (KH BZ) Antagen Societa Consortile needed to build a new hospital facility in Bolzano, Italy after an investment request from the local Bolzano medical authority. This required a new emergency power generation system that fit the specific requirements of hospital regulations and met ISO 8528-5 international standards.

Overview Challenge: Design and install new generators, digital controls, paralleling switchgear and transfer switches for life-safety and supplemental power at one of the largest private medical centers in Louisiana Solution: Cummins installed one 1750 kW diesel generator and five 1750 kW lean-burn gas generators equipped with PowerCommand® dig

Overview Challenge: Provide reliable emergency backup power supply for one of Australia’s largest public health infrastructure projects. Solution: Four C3000D5 generator sets powered by Cummins biggest low-emission diesel engine, the 78-litre QSK78G9, with a total a continuous rating of 2.2MW. The fully integrated system also incorporated a sin