New ASD Tug: Brazil Design and Brazil Built | Cummins Inc.
""
Marine

New ASD Tug: Brazil Design and Brazil Built

by Alan Haig-Brown

Cummins Vessel Reference #609


The Brazilian Port of Recife/Pernambuco is served by a powerful new ship-handling tug. The owners, Navemar Transportes e Comércio Marítimo, took delivery of the vessel, named Navemar XIII, this past September 2010.

The 30-meter azimuthing stern drive tug carries a 9.8-meter beam with a depth of 4.65 meters. The Z-drives are a pair of HRP-Series 7000 each powered by a 2200 HP (1641 kW) at 1800-RPM Cummins QSK60 engines. The tug, which is fitted with a bow-mounted hawser winch and a deck-mounted towing winch, has a 55-ton bollard pull.

Designed and built by Corema Indústria e Comércio Ltda the tug features a double chine hull that allows for good lateral movement and a raked stern profile for good backing, both of which make for improved ship handling. Electrical power is provided by a Scania-powered generator. Tankage is provided for 18000 liters of fuel and accommodation is provided for up to eight crew members.

Photos and video of the Navemar XIII are courtesy of Corema Indústria e Comércio Ltd

For further information:

Corema Indústria e Comércio Ltda
Travessa Domingos Rabelo 78, Ribeira. Salvador – Bahia
Phone: 55 11 3312-2034
Web: www.estaleirocorema.com.br

Antonio C. Colares orAline Barros
Cummins Distribuidora de Motores e Equipamentos Salvador branch
Brazil
Phone: 55 21 21963131

Waldemar Marchetti
Marine Business Manager
South Americo and Mexico
Rua Jai,
Guarulhos SP 07180-900
Brazil
Phone: 55 11 2186 4778
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...