Sarawak Slipways Builds in Aluminum | Cummins Inc.
""
Marine

Sarawak Slipways Builds in Aluminum

by Alan Haig-Brown

Cummins Vessel Reference #687

Sarawak Slipways new crewboat.

Long noted for the quality of their steel vessels, the Sarawak Slipways have recently launched an aluminum crew boat. Built to a design by Singapore-based Naval Consult Pte. Ltd., the 38 by 7.85-meter vessel has a molded draught of 1.75 meters.

With seating for 50 personnel and accommodation for a crew of eight, the vessel is powered by three Cummins engines turning fixed-pitch propellers. The port and starboard engines are Cummins KTA38M2 models delivering 1350 HP at 1900 RPM to five-blade propellers with 1050-centimeter diameters. The center engine is a Cummins KTA50M2 model delivering 1800 HP at 1900 RPM to an 1150 cm diameter prop. All four engines are coupled to Twin Disc gears (Models MGX6690SC & MGX6848SC) with 2.47:1 ratios.


The port-side Cummins KTA38-M2.

The center-mounted KTA50M2 is capable of also driving a fire-fighting pump through a front mounted power-takeoff. Auxiliary power is provided by a pair of Cummins 6BT5.9DM-powered 80sW generators. The boat is fitted with an electric bow-thruster. All five Cummins engines were supplied by the Cummins Malaysia distributor Scott & English (Malaysia) Sdn Bhd.

With three engines delivering a total of 4500 HP the crew boat can achieve a speed of 26 knots. Vessel name and owner has not yet been released. It is classed by Bureau Veritas.


Photos courtesy of Sarawak Slipways:


For further information:

Mr. YongWui Chew
Sarawak Slipways Sdn. Bhd.
Lot 2045, Kuala Baram Industrial Estate Miri, Sarawak Malaysia
Phone: 6085 605454
E-mail: [email protected]

Naval Consult Pte. Ltd.
Blk 338A, Tah Ching Road #13-35, Singapore 611338
Phone: 65 62647688

MT Chong
Sales Manager- Engine Business Unit
Scott & English (M) Sdn Bhd
Lot 1450 & 1451, Block 3, M.C.L.D., Piasau Industrial Estate,
98000 Miri, Sarawak, Malaysia.
Tel: 6085 654984
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...