Blessey Adds a New Generation Pushboat | Cummins Inc.
""
Marine

Blessey Adds a New Generation Pushboat

by Alan Haig-Brown

Cummins Vessel Reference #734

Good elevation and visibility from the wheelhouse.

With a several vessels from push boats to OSVs delivered, Joe Gregory’s New Generation Shipyard in Houma Louisiana, is now a well-recognized shipyard. Early this summer the yard delivered one of their signature 72X30-foot pushboats with a sister-ship well on the way for an September delivery.

The Lisa Gail Strafuss carries the well know Blessey Marine stack logo and is well sized and fitted out for pushing fuel barges in both the canals along the Gulf of Mexico and the Mississippi River system. A pair of grid-cooled Cummins K38-M main engines provides main power. Recognized as the industry standard for towboats of this size, the engines each deliver 1000 HP at 1800 RPM to Kahlenberge 72X58-inch propellers on 7-inch shafts through Twin Disc MG540 gears with ratios of 5.96:1.

 

And another New Generation boat ready to go to work.

The sister-ship, to be named Ben Strafuss and also for Blessey has the Cummins same main engine package. Both vessels will also be fitted with a pair of 85 kW Cummins-powered generator sets. A third vessel with a new four-cabin design by New Generation is also under contract for a December 2014 delivery.


Photos courtesy of New Generation Shipbuilding.

For further information:


Joe Gregory
Owner
New Generation Shipbuilding
440 Browning Court
Houma, LA 70363
Phone: 985 868 4088
Mobile: 985 859 5232
E-mail: [email protected]

Calvin Klotz
Vice-President Marine Division
Cummins Mid-South, Inc.
110 Airline Hwy.
Kenner, LA 70062
USA
Phone: 504 468 3535
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...