Goa’s Casino Royale at Three | Cummins Inc.
""
Marine

Goa’s Casino Royale at Three

by Alan Haig-Brown

Cummins Vessel Reference #617

The gambling ship Casino Royale.

 

In 2011 Goa’s most elaborate floating casino will celebrate three years of successful operation on the Indian province’s Mandovi River. The M/V Casino Royale wss designed by AMC Marcon of Mumbai and her builder Water Ways Shipyard with the lines of a small cruise ship. The ship has capacity for up to 400 passengers, 35 operational crew and seven professional mariners. The Casino Royale is out-fitted to meet international safety standards for a passenger vessel. Although she is equipped to sail, the 70 by 14 meter vessel remains anchored in the Mandovi River as required by local gaming regulations.

 

To meet these regulations, the vessel is fitted with a pair of KTA19-M3 main engines, rated for 500 HP each at 1800 RPM that can give her a speed of nine knots. To provide power for the five operational decks with a total of 12000-square-feet of gaming space the ship is also outfitted with three 350 kW generator sets.

For delivering passengers to and from the mainland, there are six swift feeder boats that ferry the gamers between Casino Royale’s private jetty and the vessel.

 

For further information:

 

Highstreet Cruise and Entertainment Pvt. Ltd.
Delta Corporation
Peninsula Centre, 850
Off. N.H.17, Porvorim,
Bardez, Goa, 403 521
Phone: 0832 25 12708

Girish Uttamchandani
Dy. General Manager -Shipyard business
Cummins India Ltd
Mobile: 9922956359
Fax: 91 20 2538 1591

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...