Holyhead Towing Continues Growth | Cummins Inc.
Holyhead Towing
Marine

Holyhead Towing Continues Growth

by Alan Haig-Brown

With vessels working in such diverse marine locals as the Mediterranean and Caspian Seas, the Persian Gulf and West Africa Holyhead Towing Company has build a reputation for quality vessels.

One of their particular strengths is their shallow-draft but ocean capable tugs. These boats with drafts of between two and three meters have the power to move heavy pieces of equipment and anchors. In 2009 and 2010 two more of this class of vessels have been added to the fleet. With loaded drafts of 2.5 meters the 25 by 9.5-meter vessels were built at the Hepworth Shipyard Ltd at Paull on England’s River Humber. The two vessels vary slightly in that the 2009-delivered Ak Bars has 2,200 HP while the 2010-delivered Afon Las has 2600 HP giving it a 28-tonne bollard pull and 11-knot free running speed.

Built to meet contract requirements in the shallow northern section of the Caspian Sea, the Afon Las will be flagged in Kazakhstan, whose western boarder is marked by the northern part of Caspian. It is here in the shallowest part of the Caspian Sea that the new boat will work servicing the oil industry. It is also in the shallow northern section that the Caspian is most prone to freezing. To provide a range of duties in these harsh conditions, the boat is ice strengthened and designed for carry cargo and passengers in addition to being a capable towing and pushing vessel.

The muscle for this beamy shallow-draft tug is provided by a pair of Cummins KTA 38 M1 engines each developing 1300 HP at 1800 RPM. The engines turn fixed pitch propellers in tunnels through ZF W7500 ice-classed gears with 4.939:1 reduction. Two Cummins 6B5.9D2(M)-powered 78 kW generators meet the boat’s electrical needs. A third auxiliary, this one a 188 HP Cummins 6CT8.3 D(M) engine turns a hydraulic pump to power the deck machinery and a tunnel-type bow thruster.

There is a lot to be said for experience in the design and construction of a purpose-built tug and the people at Holyhead Towing and Hepworth Shipyard say it all with this tidy tug.
 

For further information

Holyhead Towing
Phone: 44 0 1407 760111
Fax: 44 0 1407 764531
E-mail: [email protected]

Martin Stainton
General Manager
Hepworth Shipyard Ltd.

Paull
Nr. Hull
England
HU128AN
Phone: 44 0 1482 338817
Fax: 44 0 1482 338820
E-mail: [email protected]

 

 

 

 

 

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...