Repower for Dutch/Indonesian Tug | Cummins Inc.
""
Marine

Repower for Dutch/Indonesian Tug

by Alan Haig-Brown

Cummins Vessel Reference #600

 

Tugs have a way of moving around over the years. While the Indonesians bult copious numbers of tugs them selves the government run port operator PT. Pelabuhan Indonesia III is the owner of a fine big Dutch-built tug KT Anoman V. Built in the early 1990s the tug has undergone some modifications and now has three fire monitors in addition to extra bow fendering to make it better suited for port operations.

 

With recent increases in container traffic at the Port of Tanjung Perak (Surabaya) on the island of Java the need was identified by the owners to further upgrade the tug for improved handling of the container ships. The Cummins distributor of Indonesia, PT Altrak 1978, won the contract to replace the boat’s tired engines with a pair of Cummins KTA38M1 engines each developing 1000 hp at 1800 RPM. These will power the tug’s existing Schottel SRP 550 EP Z-drives (rudder propellers) with reductions of 5.059:1 and 1750 M/M fixed pitch four blade propellers.

With a beam of 8.6 meters on an overall length of 29 meters the boat made 11.8 knots on sea trials and demonstrated a 20-ton bollard pull. Capacities include accommodation for a crew of 12, 108.41 tonnes of fuel and 39 tonnes of water. A Cummins 6C-cp 135 kW generator set will meet ship’s electrical power requirements.

The repower was completed at the Semarang Shipyard.

 

For further information:

 

Mr Abdul Musi Sikki
Manager Engine Dept Head
PT Altrak 1978
JI RSC. Verteran No. 4 Binataro
Jakarta 12330
Indonesia
Phone: 62 21 736 1978
Fax: 62 21 736 1977
E-mail: [email protected]

PT Pelabuhan Indonesia III
Tanjung Perak Timur
396 Surabya
Indonesia

PT Dok Kodja Bahari
Semaran Shipyard
J1 Asahan No. 3
Semarang 50174
Indonesia
Web: www.dokkodjabahari.com

Mr Yoseph T. Arifin
Cummins Diesel Sales Corporation
8 Tanjong, Penjuru
Singapore 609019
Mobile: 65 9739 3997
Direct: 65 6661 8265
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...