Stanford Marine Grows Fleet | Cummins Inc.
""
Marine

Stanford Marine Grows Fleet

by Alan Haig-Brown

Cummins Vessel Reference #622

M/V Stanford

 

Established in 1997 as the vessel owning and operating branch of the United Arab Emirates-based Stanford Marine Group, Stanford Marine is in the midst of a major fleet expansion. In 2009 the firm acquired five vessels and acquired a company that had ten vessels on order including six new 58-meter off shore supply vessels. This brought the fleet to nearly 40 vessels and expanded the company’s operational area to include Southeast Asia.

 

The six 58-meter off shore supply vessels are being built at China’s Fujian Mawi Shipbuilding Ltd. The first of these vessels, delivered, in late 2010, was the Stanford Kite. The Stanford Condor and Stanford Osprey followed in February 2011. The other three sister vessels, the Stanford Caracara, Stanford Goshawk and Stanford Saker, will be delivered over the second and third quarters of 2011.

These are versatile vessels, described by the owners as Multi Purpose Supply Vessels, capable of transporting 162 cubic meters (cm) of liquid mud, 187 cm of bulk cement, 369 cm of water ballast/drill water, 458 cm of fuel oil and 196 cm of potable water. Liquid discharge rates with a 75-meter head include 150 cm per hour for fuel oil, 100 cm per hour for both fresh and drill water. Two pumps can offload 75 cm per hour of liquid mud while bulk cement is discharged at 13 cm per minute from two 80 psi pumps.

 

 

A fine looking ship.

 

With a 5.5-meter molded depth the hull has a 13,8-meter molded beam making possible a 376 square meter cargo deck with a 500-ton capacity. Accommodation for up to 50 workers and crew is provided in a range of single, two bunk and four bunk cabins.

 

The engine room includes an impressive suite of Cummins engines. These include three Cummins KTA19-M diesels to power the three 350 Kw main generators, one Cummins 70 kW emergency genset, and one Cummins KTA38-M1 delivering 746 kW at 1800 RPM to power an extensive fi-fi system. The system has the capacity to throw water 120 meters at a height of 45-meters above sea level from two monitors each capable of delivering 1500 cm of water per hour. One monitor is alos fitted with a double barrel for foam discharge. In the event of fire fighting, the hull and deckhouse are protected by a water spray curtain.

Main propulsion is provided by a pair of Cummins QSK60-M each delivering 2200 HP at 1600 RPM. The engines drive fixed pitch propellers in 360 degree azimuthing drives. These are Schottel SRP 1212FP. Maneuverability is further enhanced by a 500 kW Schottel tunnel thruster. The addition of these six Dynamic Positioning capable platform supply vessels will consolidate Stanford Marine’s position in the offshore industry.

 

For further information:

 

Ms. Jessy Joy
Administrator – Marketing and Contracts
Stanford Marine LLC
M1-A, Al Tayer Building,
Sheikh Zayed Road
P.O. Box 32456
Dubai, UAE
Phone: 971 4343 1055
Fax: 971 4343 5524
Mobile: 971 5045 0 0852
E-mail: [email protected]
Web: www.stanford-marine.com

Fujian Mawei Shipyard Ltd.
Phone: 0591 8368 2412 | 0591 8368 1338
E-mail: [email protected]

Linda Zhang
Cummins Inc. East Asia Marine
Manager for Southern China
Guangzhou, Guangdong
China
Phone: 86 20 3998 2999
Mobile: 86 136 0004 0695
E-mail: [email protected]
Web: www.cummins.com

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...