Experience power and reliability

Paired with innovative aftertreatment systems and cutting-edge engineering, diesel engines can operate with net zero emissions and supplement operations with biodiesel blends. Diesel allows you to go farther with less while delivering better acceleration, towing, and hauling potential when compared to gasoline counterparts. Our diesel engines offer solutions for a wide variety in the medium-duty and heavy-duty truck markets.

Next generation X15 Engine

Get a glimpse of the future

The Next Generation X15

The Next Generation X15 is the next step in the Cummins fuel-agnostic 15-liter platform. Offering up to 605 hp and 2,050 lb-ft torque, this engine demonstrates our continued commitment to the evolution of internal combustion technology.

X10 Engine
X10

Introducing the new Cummins X10, a next generation engine that bridges the gap between medium-duty and heavy-duty applications. This engine is uniquely positioned to provide efficiency and dependability

Cummins X10 Engine
Cummins announces new X10 engine

We are committed to advancing diesel technology while our markets and our customers need it to run their businesses.

José Samperio, Vice President and General Manager for Cummins On-Highway Business in North America

Truck driving out mountain towards the sun
Truck driving out mountain towards the sun
Cummins’ low-carbon fuel-agnostic engine platform strategy

The new fuel-agnostic 15-liter engine platform with advanced diesel, hydrogen and natural gas engines.

Connect with us