Integrated Powertrain | Cummins Inc.
heavy duty truck on highway
Powering possibilities

At Cummins, we are committed to empowering our customers with first-rate options to meet their needs. That’s why we’ve expanded our portfolio and partnerships over time.

Cummins has been producing engines for more than 100 years, and we now offer complete powertrain solutions - from engine to transmission to axles - with every component working in harmony.

Why integrate?

With Cummins Integrated Power, the pieces fall into place.

Higher efficiency

By optimizing factors like gear and axle ratios, Cummins Integrated Power maximizes fuel economy. Further, the integrated design reduces parts proliferation and OEM integration, thus improving the total cost of ownership.

Performance

Cummins engines offer superior horsepower ratings and productivity for their size. Eaton-Cummins transmissions and Meritor drivelines, axles and brakes ensure that power is delivered seamlessly where it’s needed.

Lower emissions

As a growing leader in emissions technology, Cummins provides integrated power solutions that support compliance with Euro VI emission standards and align with Australia's emission regulations, benefiting both our customers and the planet.

Support

With Cummins integrated power, customers can be confident that Cummins supports the entire powertrain. Assistance is never far away, with unrivaled nationwide parts and service availability.

X15 Euro VI

x15 performance engine
X15 Euro VI Performance Series

The X15 Performance series delivers more than just power and drivability. Rugged durability is ensured by the use of proven hardware while continuous improvements have resulted in reliability that provides peace of mind for truck operators. Demand nothing less than the power to perform.

x15 efficiency engine
X15 Euro VI Efficiency Series

If you want the power to save on your bottom line, then meet the X15 Efficiency Series – with fuel economy improvements over the Euro V. On top of the power to save, the Efficiency Series delivers excellent drivability and uptime that you can take straight to the bank.

Transmission and Aftertreatment

eaton cummins automated transmission
Eaton Endurant XD Transmission

Eaton Cummins 18 speed Endurant XD is designed to deliver comfort, drivability, and efficiency in on-highway applications. It is rated for engines with a maximum torque rating of 1650 – 1850 lb-ft.

single module aftertreatment
Single Module Aftertreatment

The Single Module is an ultra-high efficiency aftertreatment system. This system was developed specifically to meet customer needs first, while also meeting emissions standards.

Our Destination Zero Strategy

Road surrounded by trees next to body of water

Going further, faster

Destination Zero™

It's our mission to power a more prosperous world.

We do this by helping customers succeed through innovation and dependable products that are good for our customers and the environment.

Tied to our Destination Zero strategy, these products help customers reduce emissions.

Cummins Magazine

Worker next to Cummins generator
Check out our new Cummins APAC Magazine
Connect with us