Pushboats for the Amazon | Cummins Inc.
""
Marine

Pushboats for the Amazon

by Alan Haig-Brown

Cummins Vessel Reference #586

Angico pushing on the Amazon. Cummins photo

Transdorada Transportes LTDA, a towboat operator on Brazil’s Amazon River, has recently taken delivery of a number of Cummins-powered push boats. These include two 19.5-meter boats with twin Cummins KTA19-M3 engines each delivering 600 HP and a single 19.5-meter pushboat with a single KTA19-M3 engine. All three vessels were built at Estaleiro Rio Maguari.

The boats will operate on the Amazon River between Belem and Manaus with the 1200 HP twin engined boats pushing six to nine barges and the 600 HP single-screw vessel pushing four barges at a time. The round trip for both sets of vessels is about five days. The vessels carry the names Angico, Jatoba and Aroeira.

The DCML Norte the Cummins distributor for Amazon River area supplied the engines. Application engineers on this installation were Adriano Batista and Fabiano Pereira.



For further information, please contact:

Waldemar Marchetti
Marine Business Manager, South America and Mixico
Rua Jati
Guarulhos SP 07180-900
Brasi
Phone: (55-11) 2186 4778
E-mail: [email protected]

Olmedo Farfan
Marine Application Engineer
Cummins Inc. – Marine Business
4500 Leeds Ave
Charleston, SC 29405
Office: 843 745 1581
Mobile: 843 298 4580
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...