Reducing Emissions in Southern California | Cummins Inc.
""
Marine

Reducing Emissions in Southern California

by Alan Haig-Brown

Cummins Vessel Reference #634

M/V Christopher

In the ongoing work at reducing emissions in California and especially in the Long Beach/Los Angeles Ports, there have been a number of innovations. These have ranged from shore power for visiting ships to regulations of container trucks and container handling equipment to the Cummins-powered hybrid Foss docking tug.

In keeping with the agenda, Dan Salas at Long Beach Cruises recently repowered his 2005 Kvichak-built whale watch catamaran name Christopher. Originally powered by a pair of Cummins KTA19-M engines, the boat received a set of new EPA Tier 2 complaint QSK19 engines. The original engines were mechanical controlled while the new engines are electronic controlled fuel injection with a modular common rail system.


Port Angeles/Long Beach

Owner Sales says that the original engines had about 20,000 hours each and “never missed a beat.” He is looking forward to the same service from the new engines, which are each delivering 700 HP at 2100 RPM to ZF 350A gears with 1.5:1 ratios. This allows the Christopher to make 22 knots. The 75-foot catamaran has capacity for over 100 guests and is operated by a crew of three.

Photos courtesy of Long Beach Cruises

For further information:

Dan Salas
Long Beach Cruises
Harbor Breeze Corp
100 Aquarium Way, Dock #2
Long Beach, CA, 90802
E-mail: [email protected]

Bill Shephard
Cummins Cal Pacific
1939 Deere Ave.
Irving, CA 92606
Phone: 940 253 6070
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...