Fijian Vessel to a Practical and Versatile Design | Cummins Inc.
""
Marine

Fijian Vessel to a Practical and Versatile Design

by Alan Haig-Brown

Cummins Vessel Reference #772

The Cagivou making way.

 

In recent decades there have been great advances in design of crewboats and offshore supply vessels to meet the needs of the petroleum industry. Recently a number of nations have turned to these designs as inspiration for naval craft. Now the Government Shipping Services of the Fiji Islands have turned to a designer and a builder of offshore vessels for a new inter-island ferry.

 

 

The results are impressive. The M/V Cagivou was designed by United Ship Design of Sibu and built by Kian Juan Dockyard in Miri, also in Sarawak, Malaysia. The vessel’s 40 by 11-meter hull design owes much to contemporary offshore supply vessels (OSVs). However extensive design considerations have been included for the boat’s role as a multi-purpose utility vessel for public service. A stern ramp allows the loading of three trucks, several cars or other cargo to a 90-square-meter clear deck space. A 45-ton pedestal crane can assist with cargo loading. In the superstructure there are 40 accommodation rooms for the 16-member crew and up to 38 passengers. An additional day space is provided for up to 60 people in the salon

 

 

Pair of Cummins KTA19-M3 diesels each delivering 600 HP at 1800 RPM to four-blade 1500-m/m diameter fixed pitch propellers through Reintjes WAF364L gear with 4.482:1 ratios. This power train gives the solidly built vessel an eleven-knot speed. Auxiliaries include, two Cummins 6BT5.9D(M)-powered generators rated 80eKW, 50Hz. The vessel is also fitted with a 3.5 ton bow thruster driven by a Cummins N855M rated for 350 HP at 1800 RPM. Capacities include 160 cubic meters for fuel and 140 cubic meters of potable water. The vessel will be classed by NK.

 

 

Delivery to her owners in Walu Bay, Suva, Fiji Islands is scheduled for this July.

 

 

PDF of the GA and Profile are Courtesy of United Ship Design

 

For further information:

 

Boat Builder: KIAN JUAN DOCKYARD SDN. BHD.
Address & phone: Lot 2042, Kuala Baram Industrial Estate,
98000 Miri, Sarawak Malaysia.
Tel: 6085 605678
Fax: 6085 605455
Yard Manager: Mr. Lim Poh Meng
Email: [email protected]

 

Boat Designer: United Ship Design Sdn. Bhd.
Address & Phone: No. 4, 1st Floor, Lorong Chengal 2,
96000 Sibu, Sarawak, Malaysia.
Tel: 6084 325825
Fax: 6084 333825

Managing Director: Wong Tuong Keng
Mobile: 6012 8082825
Email: [email protected]

Engine supply: MT Chong
Cummins Scott & English Malaysia Sdn Bhd.
Lot 1524, Block 3 MCLD, Piasau Industrial Estate,
98000 Miri, Sarawak Malaysia
Tel: 6085 657850 | Fax: 6085 657252
Mobile: 6013 8336357
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...