Sub-Sea Tin Mining | Cummins Inc.
""
Marine

Sub-Sea Tin Mining

by Alan Haig-Brown

Cummins Vessel Reference #567

Thai-built tin dredges working in Indonesian waters. Photo by Khun Wanchai.

According to some reports, the world’s first mining operation in the world to use vessels for dredging ore from the sea bottom was developed in 1907 by Australian Edward Miles. He dredged the sea bottom around Thailand’s modern tourist island of Phuket to recover tin, which had been mined on the island for hundreds of years. By the 1960s some innovative entrepreneurs had begun to build iron rafts using drills to loosen the sea bottom allowing them to vacuum the residue to the surface in order to separate the tin.


Dredge controls. Photo by Khun Wanchai.

Khun Wanchai Wiriyajaree’s father was one of the innovators who developed this early equipment. When tin mining was replaced by tourism in the 1970s and 80s, Khun Wanchai moved north of Bangkok to the province of Ayutthaya where today he builds sophisticated versions of the dredges that his father helped develop. There is a steady demand in Indonesia for these dredges as they are smaller than some of the large equipment and so able to work in around obstructions.


Khun Wanchai and his wife at the fabrication shop near Ayutthya Thailand. Photo by Alan Haig-Brown.

Khun Wanchai currently has a dredge under construction that is similar to the recently delivered dredge CINTA. With over all dimensions of 80 by 16-meters, the dredge is mounted on a pontoon-barge formed from 2.54-meter diameter pipes. The cutter arms on this class of dredgers range in length from 42 to 56 meters. The rotating cutter head engine can be a small as 320 HP and is typically a Japanese truck engine. For the dredge pump on the CINTA an 850 HP Cummins KTA38 M0 is employed. Four Cummins 855 engines provide propulsion power. The two outboard of these turn shafts with props directed aft. The two inboard engines drive shafts with props directed at about 45 degrees to port and starboard of the centerline. This arrangement provides the steering and maneuverability of the big barge.

The dredged material is pumped into a series of hoppers where it is washed and vibrated to produce a concentrate that is 70-percent tin. Khun Wanchai markets his dredges as turnkey operations complete with a trained Thai crew. The crew is composed of three engineers, four maintenance workers, three vessel operators and four labourers. Remarkably the Thai crew runs the vessel on the delivery voyage nearly 2000 kilometers south from Ayutthaya Thailand to Bangka Island off the south east coast of Sumatra in Indonesia.

As in Phuket, tin has been mined on Bangka Island since at least the seventeenth century. Today it is being done with the international cooperation of technology whose design originated in Phuket.


For further information:

Wanchai Wiriyajaree
308/1 Sena,
Phranakorn Si Ayutthaya
Thailand 13110
Phone: 66 0 89 793 7997
Mobile: 66 0 85 135 7452
Fax: 66 0 3520 1440

Sathit Suwanprasert
Senior Engineer (marketing)
Cummins Diethelm Ltd.
Bangkap Huaykwang
Bangkok, Thailand 10320
Phone: 662 254 4900
Fax: 662 254 4913
E-mail: [email protected]
Web: www.dksh.com

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...