Case Studies | Cummins Inc.

Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

High speed ferry powered by Cummins QSK95 engines Tanzania’s latest fast ferry joins a fleet of vessels numerically named after the country’s majestic, dormant volcano. Built for Azam Marine, Kilimanjaro VIII is a 53m aluminum, passenger fast ferry cruising between Dar es Salaam and the historic spice island of Zanzibar. With a top speed of 37 knots at 8,000 horsepower, the vessel transits 620

As the shallowest part of the Bering Sea in Southwest Alaska, Bristol Bay is a treacherous region for vessels. Navigating strong winds amid the world’s highest tidal extremes with incredible shoals, sandbars and shallows is a required skill for commercial fishermen chasing the world’s largest salmon run. With all five Eastern Pacific species spawning in the bay's freshwater tributaries, includi

Cummins fuel cells equip world’s first commercial hydrogen fuel cell passenger ferry The only emission associated with Sea Change, the world’s first commercial hydrogen fuel cell passenger ferry, is pure (drinkable) water, produced from the fuel cells.  Built by All American Marine, the 21-meter, 75-passenger vessel is zero-emissions, hydrogen fuel-cell powered electric-drive ferry. Own

Cummins India powers world’s longest river cruise Even before its launch, M/V Ganga Vilas was destined for a rich legacy. With a sold-out manifest well into 2024, she is the first luxury cruise ship built in India. Additionally, this interesting passenger vessel was designed and built specifically to ensconce guests in the epitome of elegance and luxury for the world’s longest river cruise thro

Wherever the wind blows, Vagante wanders backed by Cummins While wandering means moving without planning, we’re certain a compass, navigational radar, and GPS guide S/Y Vagante to the most beautiful, remote, pristine places on the planet. After all, secluded islands, picturesque beaches, quaint coastal villages, and exciting passages are best explored by boat. Vagante is an incredible boat i

Magnolia One represents Turkish heritage and luxury Magnolia One is a diversion from the latest generation of yachts with exterior styling sometimes resembling white, plastic wedding cake stacks. Beckoning the golden age of yachting, Magnolia One’s graceful lines and fine craftsmanship radiate elegance, nostalgia, and Turkish charm. While dubbed a pocket superyacht, Magnolia’s DNA channels the

Following an intense storm and widespread power losses, Tulco Industrial Storage turned to Cummins to install seven generators and four transfer switches, as to keep the power on for its climate-controlled storage of mission-critical oilfield machinery.

The NEW Water wastewater treatment facility chose Cummins, after violent rainstorms left them without power for hours at a time, and two natural gas generator sets, and a DMC8000 Digital Master Control System was installed to ensure the facility continued to run smoothly through unpredictable weather conditions.

Imbued with natural light through large side hull windows, the spacious cabin of the Aquila 54 yacht power catamaran is elegant and comfortable, providing social spaces with panoramic 360° views. Offering three, four, and five cabin options as well as skipper’s quarters and galley-down layouts, this semi-custom production vessel meets an assortment of boating lifestyles. With a full-beam forwar

The newest passenger vessel for Fire Island Ferries, the “Fire Island Maid” is powered by Cummins QSL9's, with electrical power provided by a Onan MDK generator. The vessel operates primarily from Sayville to the fire island pines, taking passengers on an efficient and comfortable journey. The new Tier III compliant vehicle ferry designed by Elliott Bay Design Group is a 70-by-23-foot vessel i

The San Francisco Bay area is one of the world’s finest ports. Ships from around the world enter the Bay under the Golden Gate Bridge. Depending on their destination, they are likely to pass under at least one more of the Bay’s eight toll bridges. Not only do the bridges help both locals and visitors get to the other side of the Bay, but they also allow multiple ships to pass daily to piers throug

The Listuguj Mi’gmaq Government, an indigenous Canadian community on Quebec’s Gaspé Peninsula, has accepted delivery of a new 19.81 by 7.31-meter (65 x24-foot) combination crab trap and groundfish trawler. The vessel was designed by NAVANEX and built by Chantier Naval Forillon, both of Gaspé, Quebec, Canada. Named Ugjit Mijua’ji’jg in the Mi’gmaw language, the name means “For O

Repair, restoration and renovation of an old vessel is a significant undertaking. The reasons motivating a retrofit vary; however, in the case of Tivua, a 1982 Island Gypsy Europa MK1 retrofit, the impetus for change began in the engine room. “Before, the old engine oozed oil out of every corner,” said Rich Fricke, Tivua’s owner. “And we were so slow, running 7 - 7.5 knots and 6’s when windy. W

Pacific Haulage stands tall in the timber industry Pacific Haulage was established in Gisborne on the North Island’s east coast in 1985 to service a five-year NZ Forest Service contract. Three men – Graham Manson, Mike Treloar and Calvin Paddon who had worked together in the forestry industry in the 1970s as diesel mechanics – joined forces to establish the business with, as Treloar puts it,

The search for improved fuel economy and reliability were the key reasons Matthews Transport selected the 15-litre Cummins ISXe5 in 2013 as its standard engine brand. Based at Kojonup in a rich pastoral district 260 km south-east of Perth in Western Australia, the company is currently operating 14 ISXe5 engines in a mix of Freightliner Argosy and Kenworth K200 prime movers. The company, whic

Pricing plays big role in choosing Cummins for mains power NSW Riverina farmer Ken Brain has achieved more than a 50 percent cost reduction through switching from mains electricity to Cummins diesel generator power for irrigation pumping. Early in 2017, Brain acquired a property that was set up with mains power to drive a 100 kW line bore pump. The decision to switch to diesel generator p

  Atlas, the famed Titan in Greek mythology, is renowned for bearing the world and sky on his shoulders, a punishment inflicted by Zeus on the strongest man in the world. Somewhere near St. Louis, MO, the mortal Atlas, a 65-foot triple screw towboat, is besieged with nearly the same fate in his working life on the Missouri and Mississippi Rivers. This inland river push boat is a comm

Livestock transportation company moves millions of livestock each year Established 73 years ago, Frasers Livestock Transport may well be the oldest substantial livestock trucking business in Australia still under original ownership. Frasers today runs a fleet of 50 prime movers and 150 trailers operating as single, B-double, B-triple and roadtrain configurations. Home base is at Warwick in Q