Coastal Passenger Ferry for China | Cummins Inc.
Cummins’ Propulsion Power in China coastal ferry
Marine

Coastal Passenger Ferry for China

by Alan Haig-Brown

The Zhoushan Islands are just off shore of east China's Zhejiang province, and lie south of Shanghai on Hangzhou Bay. The main island is home to a naval base, shipyards and a port. It is a busy island with a well-developed ferry system carrying both people and vehicles back and forth to the mainland.

A fine new 690-passenger ferry, Zhoushan Islands Prosperity, has recently been added to this fleet of vessels. It is the largest ferry to date from the Hunan Xiangchuan Shipbuilding Industry Co., Ltd. Operated by a 20-person crew the sleek new twin-screw vessel will make the crossing at speeds up to 18 knots.

China Coastal Ferry Powered by Cummins

WUT Ship Co. Ltd. of Wuhan City designed the fine mono-hulled ferry. It is 65-meters in length overall with a 10.6-meter beam and a 4.3-meter molded depth. Tankage includes 8000 liters for fuel, 318 liters for water and 416 liters of lube oil. This gives the vessel a continuous operating time of 12 hours.

Propulsion power is provided by a pair of Cummins QSK60-M engines rated for 2700 horsepower at 1900 RPM and turning into an Advance Gearbox HCD1600 with a 4.75:1 reduction. Noise and vibration is reduced with the installation of a Vulkan/Wuxi flex coupling between the engine and the gear. Engine controls are by Morse Electronic Control.  The QSK60 was selected for this vessel as it meets the new Chinese emission standard GB15097.

Cummins’ QSK 60 Engine powered ferry

Auxiliary power is supplied by two sets of Cummins CCEC QSN-D(M) powered Marathon MP-H-200 Kw at 50 Hz generators. A DCEC QSB5.9 50 Kw generator set supplies harbour power.

Download QSK60 Spec sheet

 

Photos courtesy of Cummins China

For further information:
 
Hunan Xiangchuan Shipbuilding Industry Co., Ltd.
JingGang Town, Changsha City,
Hunan Province, P.R.China
Phone: 0731-82022992
 
Mr. Xindong  Xie  
East-Polar Ferry Company
Phone:  13906801295
 
Mr. Jun Yang
WUT Ship Co., Ltd  
No. 122 Luoahi Road,Wuhan City
Phone: 13886163722
 
Simon Leng
Cummins Shanghai Office
PP:  13701835643
Tel: +86 (0)21 60852701
Fax: +86 (0)21 60852666
E-mail: [email protected]

 

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...