Cummins Auxiliaries for Powerful New Off Shore Vessel | Cummins Inc.
""
Marine

Cummins Auxiliaries for Powerful New Off Shore Vessel

by Alan Haig-Brown

Cummins Vessel Reference 740

 

Reliable auxiliary power is as important to a modern off shore vessel as are the main propulsion engines. Ample and reliable electrical power is essential to the basic support systems from the galley appliances to the wheelhouse navigational devices. The Ms. Charlotte, recently delivered to Edison Chouest by Bollinger Shipyards of Lockport, Louisiana, is a powerful demonstration of this. Designated a 300 Class Deep Water Support Vessel, the vessel has a pair of GE 3,125 hp 8L250 main propulsion engines.

 

The ship has extensive electrical requirements, including cargo pumps and dual bow and stern thrusters for the Dynamic Positioning 2 system. To meet these requirements and to provide redundancy, the Ms. Charlotte is fitted with two Cummins QSK19-powered 525-kW generator sets and two Stamford PM734F 1500 kW shaft generators. To meet SOLAS requirements there is also a Cummins 6CTA8.3-DM powered 175 kW emergency generator set.

Originally built by Bollinger for their Bee Mar subsidiary, the Ms. Charlotte was one of seven vessels transferred to Edison Chouest when that firm purchased the Bee Mar fleet.

 

For further information please contact:

 

Robert Socha
Exc VP Sales and Marketing
Bollinger Shipyards, Inc.
8365 Hwy, 308 South
Lockport, LA 70374
Phone: 985 532 2554
Email: [email protected]

Sean McGavern
Territory Sales Manager – Marine
Cummins Mid-South, Inc.
5901 River Rd.
Jefferson, LA 70123
Phone: 504 648 8604
Email: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...