Cummins Power for Washington State Ferry | Cummins Inc.
""
Marine

Cummins Power for Washington State Ferry

by Alan Haig-Brown

Cummins Vessel Reference #764

The MV Sally Fox on the Seattle waterfront. (Geoff Conrad photo)

 

On March 28, 2015 King County and Vashon Island dignitaries held a ceremony on Vashon Island to dedicate the newest ferry on the Vashon Island to Seattle route. The 104 by 32-foot catamaran ferry Sally Fox will carry 250 passengers with space for 26 bicycles on the aft deck. Primary users of scheduled operation of the new vessel will be Vashon Island residents on the commute between the two terminals.

Designed by Teknicraft of New Zealand and built by Bellingham, Washington-based All American Marine Inc., the aluminum vessel is certified USCG Subchapter K for Lakes, Bays and Sounds. A pair of Cummins QSK50-M Tier 3 main engines, each delivering 1800 HP at 1900 RPM to fixed pitch propellers, power the new vessel for a 28-knot service speed.

A second vessel, building to the same design, will be delivered later in 2015. The new vessels will replace two 27-year-old boats that have been chartered for the route since 2010.

 

Geoff Conrad photo courtesy of Cummins Marine

 

For further information:

 

Joe Hudspeth
All American Marine, Inc.
200 Harris Ave.
Bellingham, WA 98225
USA
Phone: 360 647 7602
Fax: 360 647 7607
Web: http://www.allamericanmarine.com/
E-mail: [email protected]

 

Geoff Conrad
Director of Marine Business,
Cummins Northwest, Inc.
811 SW Grady Way
Renton, WA 98057
Phone: 425 235 3400
Mobile: 206 549 4689

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...