Indonesian Navy Acquires Two New Training Vessels | Cummins Inc.
Photo of Kadet-07 courtesy of Altrak
Marine

Indonesian Navy Acquires Two New Training Vessels

by Alan Haig-Brown

According to Wikipedia, “Indonesia has a total land area of 1,904,569 square kilometres (735,358 sq mi), Including 93,000 square kilometres (35,908 sq mi) of inland seas (straits, bays, and other bodies of water). The additional surrounding sea areas bring Indonesia's generally recognized territory (land and sea) to about 5 million km2.”

The nation of over 17,000 islands has 54,720 km (34,000 mi) of coastline and maintains a growing navy. In addition to national security, the navy has responsibilities for emergency services in the event of natural disasters and in patrolling the national waters to safeguard against illegal and foreign fishing fleets.

A pair of 45 by 4.25-meter patrol vessels was recently launched from the AP. Karimum Anugrah Sejati shipyard in Batam, Indonesia. Named Kadet-6 and Kadet-7, the vessels will be used in training future Indonesian Naval officers while providing patrol support to the national fleet.

Kadet-6 and Kadet-7 are each powered by a pair of Cummins KTA 50 M2 engines. With each engine generating 1800 horsepower at 1800 RPM, the vessels have a high cruise speed of 16 knots with a maximum speed of 18 knots.

Sea trials were conducted in October of 2018 and both vessels have been accepted into the fleet of the United States of the Republic of Indonesia.

For further information:

Eugene Chan
Manager Regional Marketing
Cummins Asia Pacific
8 Tanjong Penjuru
Singapore 609019
Phone: +65 6661 8265
Mobile: +65 9739 2997
E-mail: [email protected]
 
Pak Kuncoro Hadi
PT Altrak (1978), Batam Branch
Jl. Engku Putri, Komplek Sarana Industri Point
Block C1 & C2 Batam Center
Batam 29461
Phone: +62 778 – 471978
Fax. +62 778 – 432413
E-mail: [email protected]
 
Mr. Franky Sucipto
Owner,
PT. Karimun Anugrah Sejati Shipyard,
Komplek Pertokoan Trikarsa Equalita
Block C No.04 Batam Center,
Phone +62 778-7495588
Fax. +62 778-7495599
 

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...