From Korea to Bangladesh | Cummins Inc.
""
Marine

From Korea to Bangladesh

by Alan Haig-Brown

Cummins Vessel Reference #680

Ready to leave the yard for the delivery voyage.

The Bangladeshi Ministry of Shipping oversees the Bangladesh Inland Water Transport Authority (BIWTA) which is responsible for managing the country’s extensive network of inland rivers, canals and ports. (http://www.biwta.gov.bd/) The Authority also mandates and manages pilotage for those waters and vessels requiring a pilot. To undertake a wide range of responsibilities the Authority has a fleet of vessels to which they have recently added a powerful new tug.


Designed by Komac Design Tech.

Built in Pusan, Korea by the Dong Hae Shipbuilding yard to a design by Komac Design Tech Co,. Ltd., the tug is 36.6 meters long by 9.6 meters wide with a 4.2-meter depth. It is powered by a pair of Cummins 16-cylinder KTA50M2 engines each delivering 1600 HP Continuous at 1800 RPM to a pair of Schottel azimuthing drives each with a 2100 m/m four-blade propeller in a nozzle. Reduction in the drive-train is 5.858:1.The result is a bollard pull of approximately 40 tons with ample power and maneuverability to provide ship assist.


Cummins KTA50-M2: 1600 HP @ 1800 RPM Continuous

Hawser winches are located fore and aft with a towing hook also at the first deck level aft. An electro-hydraulic knuckle boom mounted on the first level cabin top will provide additional versatility for the vessel. Electrical power is provided by two 220PS x 1500 rpm gen sets and a single 72PS x 1500 rpm harbor set. Accommodation is provided for a crew of 14 persons with a total capacity of 23 persons including crew. Fuel capacity is 70 cubic meters and fresh water is 25 m3 to provide for up to 15 day voyages.


For further information:

Mr Hasan Mahmud Tarek
Chief Engineer (Marine) Co-project Director
BIWTA

Dong Hae Shipbuilding
#495-11 Gupyeong-dong
Sahagu-pusan
Korea

Koma Design Tech. Co. Ltd.
5F, 8, Hakdong-ro, 6-gil
Gangnam-gu
Seoul, Korea
Phone: 82 2 549 3161 to 3

Ben Lee
Account Manger, Marine Marketing
Cummins Korea Ltd.
Phone: 82 2 3420 0910
Mobile: 82 10 3013 0910
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...