New Catamaran "Unicat" in Argentina | Cummins Inc.
Catamaran in action
Marine

New Catamaran "Unicat" in Argentina

by Alan Haig-Brown

In September 2018, a 17-by-5 meter catamaran completed its final tests in the Tigre Delta of the Tigre on the Parana River near Buenos Aires, Argentina prior to its delivery to her Chilean owners.

The cat was designed by Eng. Emilio Noel and built by Astilleros Unidelta SA. which has a well-established reputation in a wide range of steel and aluminum workboats. The yard has a plant located in Buenos Aires with 10,000 cubic meters of open and 4,000 cu.m. of covered work space. The shipyard also has an engineering office located in the City of Buenos Aires.

Catamaran 03.jpg

The new catamaran has a capacity for 69 passengers and a three-member crew. The power for propulsion is provided by two Cummins QSB 6.7 engines, each delivering 350 HP (261 kW) at 2800 RPM.The two mains are coupled to two heavy-duty Konrad Sterndrives 680 B series. This arrangement allows the boat reach a speed of 22 knots with a range of 600 nautical miles.

The auxiliary power for the vessel services is provided by a Onan MDKBJ generator of 6 KVA. Tankage onboard includes fuel tanks with capacity for 3000 liters as well as fresh water tanks with 300-liter capacity.

The new catamaran, named Worsley, joins the tourism catamaran fleet owned by the Chilean company Hipsur SA, whose headquarters are in Natale Port, Chile. The firm provides tourist navigation services in Lake Pehoé in mountainous south Patagonia. The boat is built according to Lloyd's Register Class & Prefectura Naval Argentina standards.

 

Boat Builder:
Astilleros Unidelta S. A.
Chubut 1350, 1624 Rincón de Milberg,
Buenos Aires, Argentina
Phone: +54 11 4749 9112

Boat Designer: 
Ing. Emilio Noel
San Martín 981, Piso 4, Oficina 14, 1004 CABA, 
Argentina 
Phone: 54 11 4311 7782

Engine supply: 
Armando Tavarozzi 
HHP Sales Engines Leader 
Cummins Distribution 
Ruta Panamericana Km. 32,5 
El Talar, Buenos Aires, Argentina 
Tel: 54 11 4736-6428 
Phone: 54 11 3280-8713 
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...