South African Port Tugs | Cummins Inc.
South African Tug
Marine

South African Port Tugs

by Alan Haig-Brown

Designed in South Africa, built in South Africa, and owned in South Africa. Currently under construction the pair of 2000 HP, 19.3 by 7.25-meter tugs will be a proud addition to the fleet of South Africa’s Transnet National Ports Authority. The South African maritime design and building capabilities are well established and this new vessel will add to that strong base.

Both the dimensions and the power put these new tugs in a very popular class of tugs. Powered by a pair of Cummins’ popular K38 engines, classed IMO2, and turning Teigbridge, five-blade, B-series propellers through ZF 3750 gears with 5.950:1 ratios, the two boats will meet the diverse requirements of modern harbour work boats. With the dual engines producing 2000 HP at 1800 RPM, this functionality is enhanced by the gears being fitted with a trolling valve to allow slow-speed precision maneuvering.At the same time the props with their 1829 m/m diameter and 1472 m/m pitch will give the boat a free running speed in excess of ten knots and a solid 15-tons of bollard pull for coastal or harbour towing. Deck equipment for each vessel will include a windlass with capstan, an aft deck capstan, and a towing bollard fitted with a towing hook.

With accommodations for a crew of up to six people, the tugs will be tasked with a wide range of responsibilities from towage to pilotage work. Tankage on each boat will include 28 cubic meters for fuel, 10 m3 for water, and .83 m3 for lube oil. Auxiliary electrical power for each vessel will be provided by a pair of Cummins 4B3.9 47kW, 1500-RPM, 50kVa 400V generators.

The two tugs will be built at the Veecraft Custom Commercial Craft yard, which already has an impressive list of vessels, in both steel and aluminum, to their credit. The new tugs will be named at the time of their commissioning, currently scheduled for June 2021.
 
Rendering courtesy of Veercraft.

For further information:

Boat Owner: Transnet National Ports Authority South Africa
Contact & phone: Nazeer Slarmie  +27 060570-8688
Web: https://www.transnet.net/Divisions/Pages/NPAuthority.aspx


Boat Builder: Veecraft  Custom Commercial Craft (www.veecraft.com)
Address: Stuart McVitty, 
Shop 24, Eastern Mole Road, 
Port of Cape Town 
South Africa.  
Mobile:  +27 72 915 2003 
Phone: +27 21 7410260

Boat Designer: Naval Africa Design (www.navalafrica.co.za )
Address & Phone: 10 Rotterdam Road, 
Bayhead Kwazulu 
Natal 
South Africa 4026. 
Phone: +27 31 205 3747

Mark Sylvester
Cummins Inc.
Marine, Oil & Gas Engine Sales Manager – Africa
Tel:   +27 (0) 21 945 1888
Cell:  +27 (0) 83 415 2764
E-mail: [email protected]  
Website:  https://www.cummins.com/

Alan Haig-Brown
A. Haig-Brown & Assoc. Ltd.
Bangkok, Thailand &
Vancouver, Canada
Canada Phone: 604 520 7650
Thai Phone: 66 (0)8 5347 6206
E-mail: [email protected]
web: www.haigbrown.com
 

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...