Strategic Singapore Delivers | Cummins Inc.
""
Marine

Strategic Singapore Delivers

by Alan Haig-Brown

Cummins Vessel Reference #566

Colibri 1, photo courtesy of Strategic Marine

In the midst of a significant down turn in the worldwide demand for new crewboats, Strategic Marine is delivering vessels from their Singapore shipyard as well as their new Mexican yard. Recently delivered from the Singapore shipyard the 31 by 7.5–meter crew boat Colibri I.

Built for Indonesia’s Baruna Raya Logistics the new vessel is the fourth such vessel delivered to the Indonesian company. With seating for 50 rig workers and accommodations for up to eight crewmembers, the ABS certified vessel (type approval +A1HSC, CREWBOAT +AMS) also features a hospital with bed and its own shower/toiled and entry off the main deck.

Three Cummins KTA38 M2 engines with ABS-type approval provide power for the 24-knot vessel. Each engine develops 1200 HP at 1800 RPM with a continuous rating. The center engine is set slightly further aft than the two wing engines and has a manually operated clutch to connect its front end to a fire pump. All three engines turn propellers through Twin Disc gears. The center engine, with the fire pump, is hard mounted while the two wing engines and their gears have resilient mounts.

Auxiliary power is provided by two Cummins 6BT 5.9D (M) powered 80 kW generators. The vessel has a fuel capacity of approximately 30,000 litres of fuel in four main tanks plus one day-tank. The Colibri I also has tankage for 7,000 litres of water. Both fuel and water systems include transfer pumps.


For further information contact:

Jamie Anderson
Marketing Manager
Strategic Marine
Lot 5 Clarence Beach Road,
Henderson, W.A, Australia, 6166
Phone: 61 8 9437 4840
E-mail: [email protected]

Ku Wee Ming
Cummins Diesel Sales Corporation,
8 Tanjong Penjuru, Singapore 609019.
Mobile: 65-91135899
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...