Triple Screw, Shallow Draft | Cummins Inc.
""
Marine

Triple Screw, Shallow Draft

by Alan Haig-Brown

Cummins Vessel Reference #725

The Sea Cypress completing sea trials.

 

Over the years, Rodriguez Shipbuilding Inc, of Bayou LaBatre Alabama has probably delivered more shallow-draft tugs than any other US-yard. Their signature lugger-type tug design, with its distinctive aft cabin and wheelhouse, has a strong following amongst US Gulf Coast operators servicing near shore petro-operations. But they also built to a variety of designs.

 

This March the yard delivered a 75 by 28-foot model bow tug to Morgan City-based Garber Bros. Inc. and Sea Cypress LLC. (https://www.garberbrosinc.com/about/) The housework, built forward on the beamy hull, suggests a conventional G of M tug, it is what is below the water line that will matter to the owner and charterers. The boat has a total of nearly 2000 HP generated by three 660-HP six-cylinder Cummins QSK19 marine engines each turning a propeller through Twin Disc MGX5222 gears with 6:1 ratios. The triple screw configuration allows the design to maintain a shallow ten-foot moulded depth and, depending on load conditions, operate in as little as eight feet of water.

 

 

Named the Sea Cypress, the new boat is built to a design by yard owner Joseph Rodriguez It is a near sister to the Sea Oak delivered to Garber Bros. in 2007. The earlier boat had mechanical Cummins KTA19 engines rated at 600 HP each while the new boat has the EPA Tier 3 compliant electronic version of the 19-liter displacement engine at 660 HP each. Another modification is the addition of an elevated aluminum pilothouse providing a 38-foot eye level view to the operator.

 

Set up for both towing and pushing, the tug is fitted with SMATCO deck equipment including a waterfall type winch for anchor handling or towing. The stern deck winch can also allow the versatile tug to make up to barges for pushing by way of bridles running through stern deck rollers and side deck rollers.

Capacities include accommodation for six crew, 37,000 gallons of fuel, 6,700 gallons of water and 300 gallons of lube oil. Electrical needs will be met with a pair of 45 kW gensets.

Also under construction at Rodriguez Shipyard under yard #310 is a very shallow draft lugger tug with a pair of Cummins QSK19 engines each powering a propeller in tunnels to achieve a six-foot operating draft. The Sea Otter is slated for delivery in June 2014.

 

Photos courtesy of Rodriguez Shipyard

 

 

For further information:

 

Ronnie Totten
Operations Manager
Garber Bros. Inc.
P.O. Box 815
Morgan City
Louisiana 70381
Phone: 985 384 4511 | 985 347 2162
E-mail: [email protected]

Joseph Rodriguez
Rodriguez Boat Builders
P.O. Box 842
Bayou LaBatre
Alabama 36509
Phone: 251 824 4067
E-mail: [email protected]

Larry Neff
Marine Territory Sales Manager
1924 E I-65 Service Rd.
Mobile, AL 36617
Phone: 251 706 2754
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...