Two Engines, One Propeller | Cummins Inc.
""
Marine

Two Engines, One Propeller

by Alan Haig-Brown

Cummins Vessel Reference #650

Profile view of new China Fisheries vessel. courtesy of Rushan Shipyard

 

A recently launched patrol vessel, Zhong Guo Yu Zheng, for the Chinese Fisheries Department employs the proven technology of two engines turning into a gear with a single output to a single propeller. The Fisheries Administration Ship is 57.33-meters overall with a 8.2-meter beam and a depth of 4.2 meters. Design draft is 3.2 meters. A pair of Cummins QSK60 main engines, each delivering 2000 HP at 1800 RPM, provides propulsion power for the 500 DWT-vessel.

 

 

 

Rear view of marine gear and twin QSK60 engines

 

The two engines turn in to a massive marine gear from Hangzhou Advance Masson Marine Transmission Ltd. The gearbox combines the total of 4000 HP from the two engines. After reducing the RPM by a 7.5397:1-ratio, the power is delivered to a single shaft. Mounted on the shaft is a single 2.85-meter controllable pitch propeller. The arrangement gives the vessel speeds up to 18-knots.

 

 

 

Front view of twin QSK60 engines

 

A pair of 200 kW generators, powered by Cummins 855 engines, meets the ship’s electrical requirements. Accommodation is provided for up to 30 people. For boardings and fast patrols the ship carried two FRP speedboats, each powered by a single 200 HP outboard on the stern deck.

 

The vessel was built over a 12-month period at the Rushan City Ship Building Company Ltd. in Northern China’s Shandong Province. Also building at the yard in early December 2011 were several ships including a 6500-DWT chemical tanker as well as a pair of massive pile drivers, one with a 95-meter mast and the other with an 86-meter mast.

 

Photos courtesy: Haig-Brown/Cummins Marine except profile shot courtesy of Rushan Shipbuilding

 

 

For more information:

Ma Shu Yang
Business Department Manager
Rushan City Shipbuilding Co. Ltd.
Rushankou
Shandong, China
Phone: 0631 676 1955
Fax: 0631 676 1988
Mobile: 1350 630 9339
E-mail: [email protected]

 

Simon Leng
Marketing Manager
Cummins Shanghai Office
Shanghai, China
Phone: 86 0 21 6085 2701
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...