Big Hours, Little Wear | Cummins Inc.
""
Marine

Big Hours, Little Wear

by Alan Haig-Brown

Cummins Vessel Reference #793

The Lady Loren at work. (LA Carriers photo)

Russell Plaisance, president of Louisiana Carriers, built the pusher-tug Lady Loren at Dickie Adam’s Lockport Fabrication in 2008. At the launch, he explained that the boat was the result of five years of planning and a lifetime of experience in the maritime world of the Gulf of Mexico.


With owner Russell P. Plaisance showing the three QSK19 mains and explaining the design process. (Haig-Brown/Cummins photo)

The 82 by 29-foot Lady Loren was the seventh boat in the LA Carriers’ fleet. “ I keep my business diversified, ” Plaisance explained at the time, “We do $10 or 11 million gross per year including some business with the oil industry, but we do a little of everything else as well. We barge pipe and we once even towed baseball dirt from Houston to Tampa Bay for spring training. This new boat has a contract to tow corn syrup from Memphis to Tampa Bay.”


The Lady Loren at the time of her 2008 launch. (Haig-Brown/Cummins Photo)

Jump ahead eight years, the corn syrup plant was converted to other products and that contract disappeared. But their diversity has kept LA Carriers healthy even during the slump in the oil industry. The Lady Loren, with both towing and pushing capabilities, is currently engaged moving a pair of hopper barges on a run between New Orleans and Tampa.

The Lady Loren is a triple screw tug powered by three Cummins QSK19-M3 diesels rated at 660 HP each to give a total of 1980 HP. The engines turn three 63 by 67-inch propellers in kort nozzles.


The Lady Loren at work on the Gulf Coast. (LA Carriers photo)

“The engines had 36,000 hours on them so I decided to rebuild the middle engine,” Plaisance said recently, “Without removing the engine, my crew, together with Cummins mechanics replaced the shaft bearings, pistons and rods, heads and injectors. When we looked at the wear on the parts that came out of the engine we realized that they could easily have given us another 4,000 hours with no risk of down time.”

As a result he feels confident in leaving the rebuild of the two outside engines for another year by which time they will have a remarkable 40,000 hours each. Crediting Cummins quality Plaisance also has a very proactive service and maintenance program on the engines. Oil is changed regularly, and injectors adjusted every 10,000 hours.

LA Carriers has changed some of the fleet in the eight years since the Lady Loren was launched and they have several different engine makes in his seven-boat fleet. Plaisance is unreserved in his praise for the Cummins engines. “In future, if I have to replace an engine in one of my other tugs, it will be with Cummins,” he said.


For further information:


Mr. Russell P. Plaisance
LA Carriers, Inc.
16849 East Main
Cut Off, LA 70345
USA
Phone: 985 632 5858
Fax: 985 632 4386
E-mail: [email protected]
Web: www.lacarriers.net/

Michael Aufdermauer
General Manager Marine Sales & Engineering
Cummins Mid-South LLC
Office: 504 648-8601
Mobile: 504 220-0799
Fax: 504 734-3097
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...