Royale Floatel Lives Up to Its Name | Cummins Inc.
""
Marine

Royale Floatel Lives Up to Its Name

by Alan Haig-Brown

Cummins Vessel Reference #712

The futuristic lines of the Royal Floatel.

For harried executives, a marine cruise can offer an escape form a life of tight schedules and constant pressure. The need for a relaxing but luxurious environment was well known to the designers of M/V Royale Floatel. The Vijai Marine Shipyards, designed and carried out the conversion, from a dumb pontoon, of the Royale Floatel to a 14-room all-suite, high-end luxury floating hotel. Delivered to the owners in 2013, it is first in its segment in the country under IRS class.

With a capacity for only 60 passengers, the 60.2 by 13-meter vessel is fitted with a spa featuring Jacuzzi hot-tubs, and claims a Five Star Hotel rating with the largest room size in India. The parent company, Delta Corp. Ltd., operates a large floating casino on the Mandovi River in Goa and the Royale Flotel will cruise the same river at a relaxing eight knots. On their web site (http://www.deltacorp.in/group.html) they explain that, “The first of its kind in Goa, ‘Royale Floatel’ will be an exclusive, all-suite, luxury hotel anchored in the Mandovi river in Goa, with exclusive services for our VIP guests.


During the renovation, an emerging butterfly.

A pair of Cummins NTA855M diesels, each delivering 325 HP at 1800 RPM through ZF gears to turn 1.1-meter propellers, provides propulsion power for the floating hotel. Three more Cummins NTA855DM engines will power 330-kva gensets to meet the vessel’s extensive electrical requirements.


Photos courtesy of Vijai Marine


For further information:

Girish Uttamchandani
Business Leader – Shipyard
Cummins India Ltd
Mobile: 91 99 2295 6359
Office: 91 20 3023 3716 | Extension: 3716
E-mail: [email protected]

M/s Vijai Marine Shipyards
Rassaim, P.O. Loutolim
India
Phone: 9158998744 | 9822982122

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...