A Running Take-Out for Seaspan Cutlass | Cummins Inc.
""
Marine

A Running Take-Out for Seaspan Cutlass

by Alan Haig-Brown

Cummins Vessel Reference #702

Seaspan’s Shore Mechanic Kevin Tweedy takes great pride in the quality of fleet maintenance at the company’s Vancouver base.

“We replaced about 50-feet of bulwark around the stern on each side on the Seaspan Cutlass,” Shore Mechanic Kevin Tweedy said, “The old bulwarks were banged up and this makes the boat look better to our customers but more importantly it gives the crews pride in their vessel.”


The business end of the Seaspan Cutlass.

A steel boat can continue to serve for many years if properly maintained. Seaspan Marine is the largest towing company on the British Columbia coast. Utilizing the services of their sister companies Vancouver Drydock, Vancouver Shipyard and Victoria Shipyards, they do much of their own repair and maintenance work. The upgrade and maintenance of the 25.24 by 7.56-meter (82.8 x 24.8) Seaspan Cutlass was done at Seaspan’s Vancouver Shipyard, which was the yard that built the tug and her sisters, including the Seaspan Cavalier in 1975.


Chief Engineer Steve Erickson likes the Cummins Eliminator, “We don’t even add oil between changes.”

Both tugs have received similar upgrades. They include new MSD Sewage treatment systems, the abatement and removal of old lead-containing paint, and overhaul of the Coast Marine tow pins. Additional steel was replaced on the stern deck and around the bow in the area of the forepeak chain locker. Shafts and rudders were pulled and their bearings serviced. The fresh water tanks were cleaned and re-cemented. Kevin Tweedy, who served as owner’s rep, worked with shipyard project manager Tom Smith.

Pride and quality hold an important place in the Seaspan Marine philosophy and it is reflected on the Seaspan Cutlass in the decision to replace, like-for-like, the 850 HP Cummins KTA38 main engines during the over-haul. Tweedy stressed that the 10-year old KTA38s were a “running take-out”. In spite of having logged 47,025 hours, they were running well when the tug came in for the refit. The nozzled three-blade 79 x 75-inch props and massive Lufkin gears were retained. The engines were replaced via a hole cut in the side shell of the hull just as they had been installed a decade earlier. This efficient method of engine change kept the hours to about 20% of the total. The controls were upgraded from manual to electronic and a Maretron fuel monitor was added in recognition of the change in fuel costs over the past 10 years.


Seaspan Cutlass Captain Ray Regnier has operated other tugs with the 38-liter Cummins engines and is pleased with their reliability and their fuel consumption.

Following sea trials in late July, the 1700-HP Seaspan Cutlass returned to work with a 21-ton bollard pull towing 208 by 50-foot 2500-ton wood chip scows in tandem and triple, rail, rock and oil barges along the BC coast. The tug is fitted with a Burrard Iron Works Towing winch carrying 548.6-meters (1800 feet) of wire.

The Seaspan Cutlass: back in the water and ready for work.

Seaspan has four sets of Cummins engines currently operating in their fleet. Their first experience with the KTA38s was in the Seaspan Venture and Seaspan Tempest launched in 2003. Currently on their second set of engines both vessels had almost 40,000 hours on their original KTA38s prior to re-powering.


Photos Haig-Brown/Cummins

For further information:

Kevin Tweedy
Shore Mechanic
Seaspan Marine
10 Pemberton Ave.
North Vancouver, BC
Canada, V7P 2R1
Phone: 604 990 3391
Cell: 604 690 1714
E-mail: [email protected]
Web: www.seaspan.com

Cary Griffith
Area Sales Manager
Cummins Western Canada
18452-96th Ave.
Surrey, BC
Canada, V4N 3P8
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...