AHT from SCS | Cummins Inc.
""
Marine

AHT from SCS

by Alan Haig-Brown

Cummins Vessel Reference #569

Kitty Fox II, Photo courtesy of South China Shipyard

This past September the South China Shipyard located at Jiangmen City, Guangdong Province, China delivered another in their successful series of 4400 HP, 42 by 11-meter anchor handling tugs. The Kitty Fox II is classed BV 1 +HULL +Mach Special Service Multi-purpose AHT unrestricted navigation; the vessel is one of a continuing series. It is powered by a pair of 2200 hp Cummins QSK60-M main engines and is fitted with an anchor handling and towing winch set.


For further information:

South China Marine Ltd.
(Previous: Big Fair Industrial Ltd.)
18/F Unit All, Centre Mark II,
305-313 Queen’s Road Central,
Hong Kong
Phone: 852 2541 1282
Fax: 852 2545 4540
E-mail: [email protected]
Web: www.southchinashipyard.com

Linda Zhang
Cummins Inc.,
East Asia Marine
Guandong Province, China
Phone: 86 20 3998 2999
Fax: 86 20 3998 2180
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...