Argentine ASD Tug Launched | Cummins Inc.
""
Marine

Argentine ASD Tug Launched

by Alan Haig-Brown

Cummins Vessel Reference #774

 

 

 

 

A pair of Rolls Royce drives on the new Argentine tug Brutus.

 

Built to an Argentine design in an Argentine yard, a new 28.8 by 10-meter azimuthing stern drive tug will soon be at work handling ships in her home country. To be named Brutus, the vessel was designed by Ing. Emilio Noël and built by the Astilleros Unidelta S.A. of Buenos Aires.

 

The vessel’s 4.7 meter depth includes the two Rolls-Royce Azimuthing Thrusters, Type US 205/P20 FP. Each of these aft-mounted thrusters is powered by a 16-cylinder Cummins QSK60M diesel engine generating 2700 HP (2013 kW) at 1900 RPM. The hull form features a double chine that broadens aft to give a fine deadrise to the stern that will allow the tug to operate efficiently in both Ahead and Astern modes.
 

 

 

One of the tug’s Cummins QSK60-M main engines ready to be lifted into place.

 

With a design speed of 12-knots the 5400 HP tug is anticipated to deliver a 65-ton bollard pull. On the fore deck a combination Rolls-Royce Hydraulic Towing and anchor winch has been installed. On the aft deck, is a Mapawey Quick Release Disc-type Towing hook, Type DCX50/65 with a 65-ton release load. Other aft-deck equipment includes a three-ton 25 m/min capstan.

 

 

 

The port engine in on its bed.

 

The tug is also fitted with a diesel driven pump-set powered by a Cummins 6BT5.9-D(M) capable of delivering 200 cubic meters per hour to two monitors each capable of 100 cubic meters per hour. Two 80 kW gensets are each powered by a Cummins 6B-CP engine.

 

Accommodation is provided for up to ten crew members. Tankage includes 107.4 cubic-meters of fuel, 15.8 cu.mt. of water and 6.5 cu.mt. of lube oil. The vessel is designed and built under the rules of the Lloyd’s Register of Ships nd the Prefectura Naval Argentina.

The tug Brutus will take advantage of a flexible design to work both as a harbor and ship assist tug as well as doing coastal towing.

 

Photos courtesy of Cummins

 

Watch video at: https://www.youtube.com/watch?v=eyH2T8bl2C8&feature=youtu.be

 

For further information:

 

 

Boat Builder:
Astilleros Uni delta S. A.
Chubut 1350, 1624 Rincón de Milberg,
Buenos Aires, Argentina
Phone: +54 11 4749 9112

 

Boat Designer:
Ing. Emilio Noël
San Martín 981, Piso 4, Oficina 14, 1004 CABA,
Argentina
Phone: +54 11 4311 7782

Engine supply:
Armando Tavarozzi
HHP Sales Engines Leader
Cummins Distribution
Ruta Panamericana Km. 32,5
El Talar, Buenos Aires, Argentina
Tel.: +54 11 4736-6428
Cel.: +54 11 3280-8713

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...