Robert Allan Ltd. In Manaus | Cummins Inc.
""
Marine

Robert Allan Ltd. In Manaus

by Alan Haig-Brown

Cummins Vessel Reference #642

A Rampart 2400 under construction at the Erin yard in Manaus.

 

There are probably more Robert Allan-designed ship docking tugs under construction world wide than any other design. So it is not surprising to see one under construction at the Estaleiros Rio Negro Ltda. (ERIN Shipyard) in Manaus, Brazil. It is undoubtedly the only Rampat 2400 being built in a yard1000 miles from the sea. But then Manaus, like so much of contemporary Brazil demands superlatives for accuracy.

 

Stern view of the Rampart 2400 in Manaus.

 

The first of three Rampart 2400 ship docking tugs under construction at the yard is showing the distinctive Robert Allan Ltd. lines. From the fine underwater taper on the stern that allows remarkable bollard pull when working a line off the bow to the well-proportioned deck and wheelhouses. This is a profile familiar in a growing number of the world’s major ports. The smaller version of the Rampart design will be handling ships loading soybean at the Itacoatiara Port for Hermosa Logistics some 260 km downriver from Manaus. While the maximum length of ship to be handled at the birth is limited to 255 meters, there is typically a four-knot current at the birth. This could all make for tricky landings, but ships are provided with an experienced mooring master for the occasion. (See www.brazshipping.com.br/mapa/itacoatiara.htm)

 

Each of the tugs will be powered by a pair of Tier 2, Cummins QSK38-M engines producing 1400 HP at 1800 RPM each and turning Rolls Royce US155 model azimuth drives. Once in service these boats will do much to ease a challenging docking situation.

Haig-Brown photos courtesy of Cummins Marine

 

For more information:

Ken Harford P. Eng.
President
Robert Allan Ltd.
230-1639 West 2nd Ave
Vancouver BCV6J 1H3
Canada
Telephone: 1 604 736 9466 Facsimile: 1 604 736 9483
Email: [email protected]
Web:  http://www.ral.ca/designs/tugboats

 

Sérgio Lamarca Leite
Engineering Director
Estaleiros Rio Negro Ltda.
13, Capistrano de Abreu St., Compensa
69035-358 Manaus AM
Brazil
Phone: 55 92 9101 8552 | 92 3671 2498
E-mail: [email protected]

For further information on Cummins Marine in Manaus:

João M. N. Mendonça
Marine Business Manager
Powertech Comercial Ltda.
Av. Efigênio Sales, 1717-P.10
Manaus, Amazonas
69.060-020, Brazil
Phone: 55 92 2121 8000|8007
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...