Sibu-Built Geotech Vessel | Cummins Inc.
""
Marine

Sibu-Built Geotech Vessel

by Alan Haig-Brown

Cummins Vessel Reference #613

The Teknik Wira is outfitted with a derrick and moon pool.

Sapor Shipbuilding Industries Sdn Bnd. kept busy though 2010 delivering a range of new vessels including the handsome geotechnical vessel, Teknik Wira, from the boards of Wartsila Ship Design Singapore Pte Ltd. With her raised fo’c’sle and well-proportioned housework she presents a powerful presence that is supported by her particulars.

With a 16-meter beam carried on an overall length of 61.25 meters the vessel has impressive capabilities. Her large aft deck has a moon pool and a derrick rig as well as a five-ton crane. A pair of tugger winches and capstans are fitted to ease the movement of materials around the deck. To assist with holding position for the soil investigation works the boat has large anchors and mooring winches. In addition a dynamic positioning system utilizes Berg electric bow and stern thrusters. Tankage includes 730 cubic meters of water, 417 cu mt of fuel. Accommodation is provided for up to 50 people.

The main engines are a pair of Cummins KTA50M2 diesels delivering 1600 HP each at 1800 RPM each to Reintjes LAF675 marine gears with 7.476:1 reduction. The reduced RPM go to twin Berg controllable pitch propellers type BCP620. The combination gives the vessel a 12-knot speed light ship and 11 knots fully loaded.

Auxiliary power is provided by two 300 kW shaft generators, three Cummins 500 kWe, 28-liter VTA28-D(M)-powered generators. The designation kWe indicates the approximate engine output in the keel-cooled version. A Cummins 6BT5.9 D(M) powered gen set provided emergency power. The Scott & English facility in Sibu, Sarawak, Malaysia, supplied all engines for the Teknik Wira.

The new Port Kelang, Malaysia registered vessel was delivered to her owners, SapuraCrest Petroleum subsidiary TL Geotechnics, in July of 2010.


For further information:

Steven Yii Chu Lik
Scott & English (Malaysia) Sdn. Bhd.
No. 6A, Lorong 39
50 Jalan Ting Lik Kwong
96000 Sibu, Sarawak
Phone: 084 311807
E-mail: [email protected]

Sally Lau Ling Ling
SAPOR SHIPBUILDING INDUSTRIES SDN BHD
No. 19 & 21, 1st Floor

Jln Chengal
96000 Sibu
Sarawak Malaysia
Tel: 6084 324513
Fax: 6084 324400
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...