Steiner Delivers Fourth Z-Drive Pushboat | Cummins Inc.
""
Marine

Steiner Delivers Fourth Z-Drive Pushboat

by Alan Haig-Brown

Cummins Vessel Reference #565

Arne Christiansen, photo courtesy of Steiner Shipyard

The final, for now, delivery in a series of four 120×34-foot 3200-HP Z-drive towboats was completed at Steiner Shipyard in Alabama. The innovative vessels were built for Southern Towing of Memphis Tennessee.

As with the other three vessels the Arne Christiansen is powered by a pair of Tier 2 compliant Cummins QSK50 mains, each rated for 1,600 HP at 1800 RPM provides the power. The two engines are mounted aft on the main deck level. They turn short four-foot shafts to HRP Z-drives carrying 74.8-inch (1900 m/m) propellers in steerable nozzles.


Arne Christiansen, photo courtesy of Steiner Shipyard

The use of steerable nozzles in the Edward Shearer designed vessels was a significant departure for Mississippi pushboat design. Kenny Williams, pilot on the David Stegbauer delivered in December 2008, Kenny explained some of the advantages in the Z-drive boat’s handling while steering around the big bends up-bound on the river from New Orleans. “With a rudder boat I would be putting on 40 to 45 degrees of rudder on both sides, but with the Z-drive I only put about 20 degrees on the drive that is on the inside of the turn while the other drive pushes ahead.”

When steering down river with loaded barges he said, “With a rudder boat the biggest danger in flanking a bend is lovins your stern to the current: with a Z-drive you can just turn it back in.”


For further information:

Marco Angelini
Sales and Marketing Associate
Steiner Shipyard, Inc.
P.O.Box 742
8640 Hemley Street
Bayou La Batre, AL 36509
Phone: 251 824 4143
Fax: 251 824 4178
Cell: 251 680 6110
E-mail: [email protected]
Web: www.steinershipyard.com

William Stegbauer
President
Southern Towing Company
1874 Thomas Road
P.O. Box 411
Memphis, TN 38101
Phone: 901 386 2644
Fax: 901 386 1119
E-mail: [email protected]
Web: www.southerntowing.net

Edward L. Shearer, P.E.
Shearer & Assoc.
Naval Architects
3663 Nasa Road One
#608 Seabrook, TX77586-6319
Phone: 281 532 2080
E-mail: [email protected]

Peter J. Slootmaker
General Manager
HRP USA, Inc.
419 Avenue of the States
Chester, PA 19013
Web: www.hrp.nl

Larry Neff
Marine Marketing Manager
Cummins Mid-South Inc.
3422 Georgia Pacific Ave.
Mobile, AL 36617
Phone: 251 473 3095
Fax: 251 473 6657
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...