Get your suspension ready for a smooth ride | Cummins Inc.

Get your suspension ready for a smooth ride

By Cummins Inc., Global Power Technology Leader

Get your suspension ready for a smooth ride

Your vehicle’s suspension system does more than just provide a comfortable ride; it plays a critical role in keeping your vehicle stable, aligned, and performing at its best. Every bump, pothole, and turn puts pressure on suspension components. Over time, wear is inevitable. 

That is why regular suspension maintenance—and knowing when to replace key components—is key to extending vehicle life, improving ride quality, and preventing costly repairs down the road.

At Cummins, we are proud to offer trusted aftermarket suspension solutions through our Meritor, Euclid, and GAFF brands. From bushings and shocks to air springs and hardware, we provide suspension components engineered to perform in real-world conditions.

Here are five key areas to check and maintain to ensure your suspension is ready for a smooth ride:

1. Bushings: the silent protectors of your suspension

Bushings may be small, but they serve a big purpose. They are rubber or polyurethane parts designed to absorb vibrations and reduce friction between suspension parts. They protect your system from wear while keeping everything aligned and operating quietly.

Watch for these warning signs:

  • Clunking or knocking sounds over bumps
  • Uneven tire wear
  • Excessive movement in suspension components

When bushings wear out, the ride becomes rougher, handling gets looser, and the suspension becomes less responsive. Replacing worn bushings restores ride comfort and helps avoid further damage to surrounding parts.

Tip: Bushings should be inspected regularly and replaced at the first signs of cracking, tearing, or separation.

2. Shocks: ensuring stability and control

Shocks absorbers are essential for keeping your wheels in contact with the road. They manage the impact of bumps and dips while minimizing vehicle bounce and sway. When your shocks are in good shape, your vehicle handles better and stops more predictably.

Signs it’s time to replace:

  • Excessive bouncing after hitting a bump
  • Fluid leaking from the shocks
  • Nose diving or swaying during braking and turns
  • Increased stopping distance


Tip: Shocks should be inspected every 50,000 miles, or sooner if you notice symptoms. When replacing your shocks, they should be replaced in pairs to maintain suspension balance Replacing worn shocks improves safety, ride comfort, and overall handling.

3. Air springs: comfort and load Support

Air springs play a crucial role in maintaining consistent ride height and vehicle stability, particularly when carrying heavy loads. They automatically adjust to varying road conditions, ensuring optimal comfort and load support.

Signs of air spring failure:

  • Sagging suspension on one side or corner
  • Uneven ride height
  • Air leaks or visible cracks in the rubber

Driving with a compromised air spring can strain your entire suspension system and reduce ride comfort. Replacing damaged air springs is key to preserving vehicle balance and preventing further wear on axles and other components.

Tip: Routinely check for visible wear, air leaks, and listen for hissing sounds that indicate escaping air. When replacing your air springs, it’s recommended to replace your shocks as well to prevent premature failure.

4. Springs: the backbone of your suspension

Steel springs—whether leaf or coil—are the foundation of your suspension. They carry the weight of the vehicle and absorb road shock to provide a smoother ride and better handling.

Signs it’s time to replace springs:

  • Drooping or uneven ride height
  • Poor handling or excessive body roll
  • Broken or cracked spring leaves

When springs begin to sag or break, the entire suspension can suffer. Replacing worn springs not only restores ride height but also ensures safe handling and load control.

Tip: Inspect the full length of each spring for cracks, corrosion, and misalignment, especially after winter driving, which can accelerate wear.

5. Fasteners: small components, big impact

Fasteners, such as bolts, nuts, and clips, hold your entire suspension together. While they may seem minor, these components are essential for keeping everything securely mounted and properly aligned.

Why fastener maintenance matters:

  • Loose or corroded fasteners can cause suspension misalignment
  • Missing or damaged bolts may lead to premature component failure
  • Regular torque checks prevent system loosening over time

Corrosion from winter salt and moisture can weaken fasteners. Routine inspections and replacements are a small investment that pays off in suspension longevity and vehicle safety.

Tip: During every inspection or part replacement, verify that all fasteners are properly tightened and show no signs of rust, wear, or stripping.

Take the guesswork out of suspension maintenance

Knowing what suspension components are on your vehicle and understanding what needs service should not be a guessing game. That is why we offer helpful tools like the Identification Xact Search and the Visual Search tools on MeritorPartsXpress.com.

With these tools, you can:

  • Identify suspension parts by make and model
  • Cross-reference part numbers
  • View exploded diagrams for accurate identification
  • Access installation guides and product specs

Whether you are ordering a replacement bushing or rebuilding an entire suspension system, these tools help ensure you get the right part the first time, saving you time and reducing downtime.

Why Meritor and Euclid aftermarket suspension components?

With decades of experience and a reputation for reliability, our suspension components are built to handle the demands of commercial and heavy-duty vehicles. When uptime, safety, and performance matter, we deliver. What you can expect:

  • Durability you can trust – Components engineered to OEM standards
  • Wide application coverage – Fitment for a broad range of truck models
  • Fast availability – In-stock parts shipped quickly to minimize downtime
  • Support and service – Backed by a knowledgeable team ready to help

When it is time to replace worn suspension parts, don’t compromise. Meritor and Euclid offer the performance, reliability, and value your fleet depends on.

Ready to roll smoother?

Proactive suspension maintenance is one of the smartest ways to protect your vehicle, improve ride comfort, and reduce long-term repair costs. By keeping an eye on components like bushings, shocks, air springs, and fasteners and replacing them when needed, you will stay safer on the road and avoid costly downtime.

Schedule a post-winter inspection today with your service provider or fleet maintenance team.

Then visit meritorpartsxpress.com to browse high-quality aftermarket suspension parts, identify your components with the Visual Search Tool, and order everything you need for a smoother ride.

Author Profiles

Cummins Office Building

Cummins Inc., Global Power Technology Leader

Cummins Inc., a global power leader, is committed to powering a more prosperous world. Since 1919, we have delivered innovative solutions that move people, goods and economies forward. Our five business segments—Engine, Components, Distribution, Power Systems and Accelera™ by Cummins—offer a broad portfolio, including advanced diesel, electric and hybrid powertrains; integrated power generation systems; critical components such as aftertreatment, turbochargers, fuel systems, controls, transmissions, axles and brakes; and zero-emissions technologies like battery and electric powertrain systems. With a global footprint, deep technical expertise and an extensive service network, we deliver dependable, cutting-edge solutions tailored to our customers’ needs, supporting them through the energy transition with our Destination Zero strategy. We create value for customers, investors and employees and strengthen communities through our corporate responsibility global priorities: education, equity and environment. Headquartered in Columbus, Indiana, Cummins employs approximately 67,400 people worldwide and earned $2.8 billion on $33.7 billion in sales in 2025.