Brazil’s Inace Shipyard Delivers Second GPA FSV | Cummins Inc.
""
Marine

Brazil’s Inace Shipyard Delivers Second GPA FSV

by Alan Haig-Brown

Cummins Vessel Reference #660

The Siem-Carajas on sea trails.

 

The second Guido Perla & Associates designed fast supply vessel has been delivered from Brazil’s Inace Shipyard. Named Siem Carajás, the 50-meter (164-foot) by 10-meter aluminum vessel features a large forward cargo shelter. There is also a large 28.5 by 7.8-meter open after deck. Liquid capacities include: ships fuel 22 m3, cargo fuel oil 64.6 m3, ship’s potable water 17.4 m3, potable water cargo 65 m3. Deck cargo capacity is 250 metric tons. The maximum design speed, light boat, is 25 knots with a 21-knot service speed when 175 mt DWT. Maximum deadweight is 350 mt.

 

 

 

 

Four Cummins KTA50-M2 each delivering 1800 HP at 1900 RPM to 1.2-meter propellers through Twin Disc gears provide propulsion. A pair of Cummins-powered 99 kW generators meets the vessel’s electrical needs.

 

 

Photos Courtesy of Cummins Brasil Ltda

 

 

For further information:

 

Alan Haig-Brown
A. Haig-Brown & Assoc. Ltd.
New Westminster, B.C., Canada
CAN Mobile: 604 377 1577
Web: www.haigbrown.com

Waldemar Marchetti Sobrinho
Marine Business Executive Manager – South America & Mexico
Phone: 55 11 2186 4778
Mobile: 55 11 7609 1033
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...