Cummins Case Studies
We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.
Custom built for offshore tournaments With large cockpits and custom configurations, Henriques Yachts produces canyon-capable fishing machines with the muscle and seakeeping capability of a real, rough-water boat. Capable of venturing out safely in the chop over 100 miles to reel in a big trophy tournament fish, the strong and solid Henriques hull is strategically designed to endure ha
The converted VLCC Ariake will offer substantial oil storage with Cummins marine propulsion. FPSOs are big, expensive pieces of equipment As the search for oil has moved into deeper waters with more distance to shore-based facilities, Floating Production Storage and Offloading vessels have become essential tools in the process. Typically, the large FPSO is stationary with a number of wells f
Overview Challenge: Provide power system technologies for a completely off-grid microgrid solution in a remote location but at a commercial scale. Solution: An integrated renewable power system with two of Cummins 72 kW diesel generator sets. Result: A fully integrated remote microgrid energy solution that has been in oper
Overview Challenge: Provide power for a remote marina with load demands varying between 5 and 500kW while impacting year-round operating costs to increase maximum efficiency and allow the system to run completely on renewable energy when the system is not at peak capacity. Solution: An integrated microgrid power system using Cummins Power
Welcome aboard SeaVee Boats’ new flagship 450z center console. Offering a combination of luxury and style, the 450z offers is a solid fishing machine that’s easy to maneuver with offshore performance bolstered by Cummins marine auxiliary. Designed with a sensible, safe deck arrangement, the 450z is equipped with all around zail fishing rods and four live wells to reel in a big tournament catch.
An international partnership to build a new inland river tanker with Cummins marine propulsion proves that the right partners can accomplish amazing results. M.S. Servio inland river tanker travels the Danube for complete assembly International boat building has become an accepted practice, with fishing boat hulls being built in Poland and towed to Norway for complet
Gamefisherman's largest build yet Game on! The tournament-winning boat builders from Gamefisherman have launched their largest build to date, the 50 Express. Equipped with Onan generators, the 50 Express is personalized for tournament sportfishing with customizable options, cold-molded mahogany and is available in three styles: coupe, walkaround and flybridge. The raised teak
Combining elegance with sporty lines and an incredible layout, the Prestige 590 offers the latest innovations with an impeccable megayacht finish in 61 feet. With the luxury of a family yacht designed like a vacation residence on the water, the Prestige 590 provides the atmosphere of a private island retreat. Promising a dream at sea while always feeling at home, Garroni Design’s sle
Red sky at morning, sailors take warning. Red sky at night, sailors' delight. Red Sky at dawn? A stunning Swan. The ancient meme oft repeated by mariners is a rule-of-thumb weather forecast. Based on the reddish glow of the morning or evening sky caused by haze or clouds related to storms in the region, a red sky provides prediction for bad weather later in the day. Red Sky at Dawn: A
For nearly a century, the rugged coast and islands of Scotland were served by the handy little steam freight boats known as Puffers. They carried manufactured goods out to villages and farm produce back to the mainland. The recent delivery of the 27-by-9.7-meter Havara shows just how dramatically small coasters have developed over the past two generations. In fact, apart from that their role as a
Joey Rodriguez has seen the ups and downs of the boat building business at his Rodriguez Shipbuilding in Coden Alabama. For a time, there was huge demand for big steel Gulf Shrimp boats and then the oil industry ramped up and kept him busy with a variety of tugboats. Then came the crash in oil prices and the crash in demand for towboats. Joey shuttered his yard for a year and a half. “I didn’t
Bunkering ports around the world have long used a variety of small tankers or tug and barge combinations to deliver fuel to visiting ships. Mostly this was heavy oil, but recently a new breed of bunkering vessels is emerging to deliver clean burning LNG to modern ships with dual-fuel capabilities. The fall of 2020 will see a fine new addition to this fleet servicing cruise ships in Florida and
It has been said that if you want a versatile, practical, and safe boat, go to an islander. With multiple generations on the Isle of Škoj in the Adriatic off the Croatian city of Split, Luka, the youngest of the Colnago family, is a noted designer and builder. His latest work, the Colnago 45 Pilot, is one of his most versatile yet. A lot of Luka’s boats are high-end, high-speed, pleasure and to
Like many fishermen, Justin Yager is interested in the responsible harvesting or marine resources. “We don’t need to be fishing the crabs right up into their molt stages,” he said recently. Similarly, he saw the common sense of rebuilding the Gulf Shrimper B.J. Thomas when the boat had a serious fire at Newport, Oregon. Built in 1976 at Marine Builders in Mobile, Alabama the boat found its way
Overview Challenge: Red Cross Hospital in Cordoba, Spain needed to replace an older outdated backup genset with a new genset that provided 220 kva. In addition, the removal of the old genset and installation of the new backup genset needed to take place within a 24-hour period without leaving the hospital at risk during an outage. Solution: The
In 2020, Kubota unveiled its largest tractor to date – the 19,510 lb. / 8550 kg M8. Its big features – power, reliability, comfort and value. Power comes in the form of a 180 hp (134 kW) or 200 hp (149kW) Cummins B6.7 Performance Series engine. As Cummins’ most popular product, with over 15 million B Series engines built since its introduction, the B6.7 represents next generation engine technol
Overview Challenge: Provide cogeneration solution to Varegro, a horticultural company in Ootrozebeke, West Flanders. Solution: Install Cummins C2000N5CD 2MW HSK78G gas generator to provide additional power along-side vast cost and energy savings. Result: A range of energy needs were met in addition to converting remaining waste
Overview Challenge: Supply Belgian tomato grower Desmet with combined heat and power system delivering on agreed level of electrical and thermal energy. Solution: Design, build and provide Desmet with an energy service contract. Result: Reduced heating costs and emissions without increasing cash-flow and incurring the costs of i