From China to Peru | Cummins Inc.
""
Marine

From China to Peru

by Alan Haig-Brown

Cummins Vessel Reference #580

Peruvian tug on seatrials in China. Cummins photo

A 26.5-meter Z-drive tug has recently been delivered from the Jiangsu Wuxi Shipyard Co., Ltd. in China to a Peruvian owner Trabajos Maritimos S.A. The shipyard is located inland from Shanghai on Lake Thai near the town of Wuxi and the Jinghang Grand Canal. Trabajos Maritimos is a comprehensive marine organization offering every thing from port agency services, terminal operations, pilotage and towing.

The new tug, delivered in November of 2009, is powered by a pair of Cummins QSK60 engines each delivering 2200 HP at 1800 RPM to HRP Model 7111 WM (P3) azimuthing drives with 6.681:1 reduction. The tug is designed with the forward hawser winch typical of modern docking tugs. A pair of Cummins 6BT5.9DM powered genset each provide 100kW of electrical power while a smaller 38 kW set for harbout service is powered by a Cummins 4BT3.9DM genset.


For additional information:

Jingsu Wuxi Ship Yard Co., Ltd.
18 Xinhui Rd.
Wuxi Jiangshu, China

Linda Zhang
Marketing Manager
Cummins Inc.,East Asia Marine
Guangzhou, China
Tel: 0086 20 39982999
Fax: 0086 20 39982180
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...