Turkey/Norway Diesel-Electric-Battery Ferry | Cummins Inc.
Norway IMO III Ferry
Marine

Turkey/Norway Diesel-Electric-Battery Ferry

by Alan Haig-Brown

With a rugged coastline and many fjords to cross Norway has become a world leader in progressive ferry design. Turkey, with a skilled work force and broad marine experience has become a leader in ferry construction. Put the two together and you have the teamwork that results in the Basto series of RO-RO ferries.

The latest in the class, Basto VII, to be launched in December of 2019, will be powered by four Cummins QSK50 IMO Tier III diesel-powered generator sets, two in each end and each producing 1290 kWm. The electrical system will power motors mounted atop two 360 degree electrically driven azimuth thrusters, one in each end of the ferry.

These are turning Kongsberg AZP100-L-CP-F TME22 azipull drives.  Kongsberg explains, “Combined with the proven high propulsive and hydrodynamic efficiency of the Azipull this will be a winning combination, especially as there is a further small gain in mechanical efficiency by eliminating the upper gearbox. Space requirements in the thruster room are reduced because the new thruster is compact, the PM motor lying within the diameter of the mounting flange giving a small footprint and avoiding the complication of a coupling and foundations for the separate motor of a conventional Z or C drive electric configuration.”

The 143.24 by 20.7-meter ferry, like her sisters, will be highly maneuverable for the 30-minute crossings across Oslofjord between Moss and Horten at about 13.5 knots. The ferry will carry up to 500 passengers and 200 cars. Tankage will include 160 cubic meters for fuel, 60 cubic meters for water and 2400 liters of lube oil.  The new Double Ended RO-RO battery ferry will be classed “EU Class C” MM139FD. Main Engines & SCR System will be classed by: DNV GL +1A, FERRY B. BATTERY (POWER), E0, ICE C, R3 (nor).

Download Cummins IMO III Solution Brochure

Photo courtesy of Bastø Fosen AS

For further information:

Willy Pettersen
Bastø Fosen AS
Rustadbrygga 5
Postboks 94
N-3191 Horten
Phone: 4741519170
E-mail: [email protected]  

Çağlar Polat
Sefine Denizcilik Tersanecilik Turizm San. ve Tic. A.Ş.
Hersek Mahallesi İpekyolu Caddesi
No:7 Altınova –YALOVA / TÜRKİYE 77700
Phone: 0090 553 017 01 95
E-mail: [email protected]

Elshad Asadi
Marine Sales Engineer / marin Satış Mühendis


Cummins Turkey Motor Güç Sistemleri Satış Servis Ltd. Şti.


İstanbul Anadolu Yakası Organize Sanayi Bölgesi
1.Sokak No:5 PK : 34953 Aydınlı, Tuzla -  İstanbul / TURKEY
Harita: N 40°53’05”  E 29°23’06”
 
Phone: +90 216 581 73 69
Santral: +90 216 581 73 00
Fax: +90 216 394 86 08
Mobile: +90 530 202 58 80
E-mail: [email protected]
Web: www.cumminsturkey.com

 

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...