Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

 When Khun Namchai Sakunchoknamchai was seven years old he like cars. So he built himself one out of wood. Decades later, he was building those big beautiful custom tour buses that are a feature of Thai roads. When he wanted a 30 million baht machine for shaping rolled aluminum sheet, he designed and built one for less than nine million THB. This machine is just one of the impressive array of

A recent report by the Ghana Ports and Harbour Authority states, “Total cargo traffic for both ports (Tema and Takoradi) grew from 19,459,834 tonnes in 2016 to 22,086,626 tonnes in 2017, registering a 13 per cent increase. Transit cargo in both ports also increased from 944,081 tonnes in 2016 to 1,249,336 tonnes in 2017, a rise of 32 per cent. Container traffic for both ports rose from 942,463 TEU

 Thousands of people travel Alaska on mega-cruise ships each year, but only a handful get to cruise Alaskan waters on the immaculate M/V LISERON. Built in Seattle in 1952 by the US Navy as a minesweeper she was sold to France, but returned to Seattle in 1990 after being lovingly converted to yacht-class in Florida. The late Michael Allan McIntosh, philanthropist and environmentalist, found

Fish companies from New Zealand to Russia (currently 24 large and ultra large Russian vessels) and Iceland to the USA as well as Greenland and now Canada have chosen the Norwegian firm Skipsteknisk when it comes time to design a new vessel. The firm has garnered a reputation for designing and overseeing the construction of vessels that integrate the most up to date technology from deck equipment t

With Weeks Marine reaching their 100th anniversary in 2019, it is fitting that they would be running one of their crew boats with Cummins’ latest marine engine, the X15 as 2019 also represents the centenary for Cummins. Weeks began as a stevedoring company in the Port of New York. Today their dredging and other operations span much of North and South America. Originally, the company’s floating

Crinklaw Farm Services Inc worked alongside Cummins to develop a suitable long term power solution for their Global Unmanned Spray System (GUSS). That solution is the Cummins QSB6.7 engine, which now powers the world’s first and only autonomous orchard sprayer. The QSB6.7 is a fully integrated system rated at 173hp (129 kW) with cooled exhaust gas recirculation (EGR) and a High Pressure Common

According to Wikipedia, “Indonesia has a total land area of 1,904,569 square kilometres (735,358 sq mi), Including 93,000 square kilometres (35,908 sq mi) of inland seas (straits, bays, and other bodies of water). The additional surrounding sea areas bring Indonesia's generally recognized territory (land and sea) to about 5 million km2.” The nation of over 17,000 islands has 54,720 km (34,000 m

As the second largest producer of almonds in the world, Australia is seeing a dramatic increase in greenfield almond farm developments across Victoria, New South Wales and South Australia. The Almond Board of Australia is predicting orchards will grow to sprawl across more than 50,000 hectares (124,000 acres), producing an annual crop worth more than $1 billion by 2025. The Almond Board of Aust

Australian spray equipment manufacturer Goldacres is well known for providing a wide range of spray equipment, from its 2-litre hand held compression sprayer through to the 8,000-litre broad acre, self-propelled Super Cruiser. In 1996, Cummins was chosen as Goldacres’ driveline partner during the development of its first self-propelled Crop Cruiser sprayer. Launched in 1999, Goldacres’ flagship

In September 2018, a 17-by-5 meter catamaran completed its final tests in the Tigre Delta of the Tigre on the Parana River near Buenos Aires, Argentina prior to its delivery to her Chilean owners. The cat was designed by Eng. Emilio Noel and built by Astilleros Unidelta SA. which has a well-established reputation in a wide range of steel and aluminum workboats. The yard has a plant located in B

Paraguay’s Tsuneishi Shipyard, a subsidiary of the Japanese firm of the same name, recently delivered the powerful towboat Tebicuary 3 to her owners Navegación del Sur S.A. (Navesur) in June of 2018. The new vessel is a near sister-ship to the 2015-delivered Ceasar Primo for a different owner. The newer vessel will also work on the Paraguay-Paraná River system that provides marine access to lar

Cummins Vessel Reference #818 At work on the river. Most visitors to Bangkok will experience a ride on the Chao Phraya Express boats. These long, sleek, wooden, commuter boats, with their dramatically raked bows, are a staple of the river’s traffic. They can also be very crowded and, with many stops, a bit of a challenge to the tourist. A popular alternative is the tourist boats. These vessel

Cummins Vessel Reference #839 As the crane swing on its 60-foot diameter ring, the tug had to be lifted to clear winches and containers on the barge deck.   The ownership of the Canadian firm Island Tug and Barge has changed with the purchase by the US parent company Tidewater Inc. The firm is now known as Island Tug. https://www.islandtug.com/ The second tug, with the hull a

Cummins Vessel Reference #840 I profile the Fathom offers a pleasingly capable look.   Contemporary composite cruisers are designed so similarly that finding your boat in a crowded marina can be a challenge. Such will not be a problem for owners of the latest incarnation of the well-regarded Fathom 40 and 43.   Builder Roy Parkingson at the galley table. Long t

Cummins Vessel Reference #592 Tennessee’s Serodino, Inc. recently built one of their popular Tiger class push boats for their own use. The M/V Charger, like others in the class, is 51.5 by 22.5-feet with a 5-foot 6-inch draft. The hull is constructed of 3/8-inch plate with 1/2-inch plate over the propellers and bilge knuckles. Designed in house, the boat is a sister to a number that the company

VEHICLE YEAR: 1993 MAKE: Toyota MODEL: Land Cruiser BUILDER: Proffitt's Resurrection Land Cruisers (Click here to download a printable poster from this Cummins Repower project.) DRIVETRAIN Cummins Repower R2.8L Turbo Diesel Toyota H55F transmission Part time 4WD transfer case SUSPENSION 4 link / 3link with coils TIRES/WHEELS 285/70R17 Ma

VEHICLE YEAR: 1979/1982 MAKE: Toyota MODEL: BJ40/BJ42 Land Cruisers BUILDER: Custom Works (Paso Robles, CA) Travis Smith with Steven Ploog & Nathan Stuart (Click here to download a printable poster from this Cummins Repower project.) DRIVETRAIN Cummins Repower R2.8L Turbo Diesel nv4500 to stock Transfer Case and twin sticks all adapter parts from Advance