Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

Cummins Vessel Reference #739 Dann Marine Towing, LC., is a fifth generation family owned and operated tugboat company based in Chesapeake City, MD. The model-bow twin-screw tug Sea Coast was built at Rayco Shipbuilders in 1980 and is one of Dann Marine’s 18-tug fleet. She is 65 feet overall with a 24-foot beam and an 8.9-foot draft. She carries 16,000 gallon fuel and 5,000 gallons of water.  

Cummins Vessel Reference 740   Reliable auxiliary power is as important to a modern off shore vessel as are the main propulsion engines. Ample and reliable electrical power is essential to the basic support systems from the galley appliances to the wheelhouse navigational devices. The Ms. Charlotte, recently delivered to Edison Chouest by Bollinger Shipyards of Lockport, Louisiana,

Cummins Vessel Reference #738 A fine new Norwegian longliner built in Poland.   In June of 2013 the Polish Shipyard Poltramp had begun construction of a 20.99 by 8.5-meter longliner for a Norwegian customer.   In August of 2014 the new vessel, having completed successful fishing trips, travelled to Trondheim, Norway for exhibition at the Nor-Fishing trade show on behal

Cummins Vessel Reference #756 The tug Norman O on the hip of an Alaskan log barge. It has been said that, “There is no reason to design or build an ugly boat.” This is clearly a dictum that those who designed and built the Noman adhered to. Built in 1970 as the Duncan Foss by the Albina Shipyard under hull#419, at Portland, Oregon. The tug has a fine shear that sweeps down the 75-foot length fr

Cummins Vessel Reference #735 Another 23.5-meter 1200 HP tug ready for launch.   The Sibu, Sarawak based Rajan Maju Marine Industry yard continues to offer their successful handy size tug available on prompt delivery. The 23.5 by 7.315-meter tug has a single chine 3.048-deep hull. The keel is fabricated from 12 milometer steel plate while the bottom, sides and deck are all nine

Cummins Vessel Reference #737 One of six: ready to go to work.   Ngieng Hock Sii of Rajang Maju Marine Industries reports that his yard has delivered a half-dozen Cummins-powered tugs to Coastal Contracts Bhd. of Sabah, Malaysia. Coastal is a Malaysia based firm offering services that “include build, charter, repair, maintain and trade of marine vessels, ranging from tug boats, o

Cummins Vessel Reference #734 Good elevation and visibility from the wheelhouse. With a several vessels from push boats to OSVs delivered, Joe Gregory’s New Generation Shipyard in Houma Louisiana, is now a well-recognized shipyard. Early this summer the yard delivered one of their signature 72X30-foot pushboats with a sister-ship well on the way for an September delivery. The Lisa Gail Strafu

Cummins Vessel Reference #732 The Captain D: all dressed up and ready to go. Established in 1928 by George Lyon Sr, Lyon Shipyard today occupies 30 acres of waterfront near downtown Norfolk Virginia. Norfolk Tug is based in the same area and takes pride in operating a fleet of tugs from the 1970s and ‘80s that they proudly designate as “vintage steel”. They also have an aggressive program of

Cummins Vessel Reference #727 A recently launched trawler is fitting out alongside at Mahachai Dockyard. After a bit of a lull in construction, the Mahachai Dockyard had six trawlers in various stages of completion in mid-April of 2014. Ranging in size from three 45-meter, one 38.5-meter and two 25-meter vessels all six will be powered by Cummins KTA38 engines generating 800 or 1000 HP dependin

Cummins Vessel Reference #730 The Erin C Grenon on the Mississippi River.   Over the past decade Blessey Marine has taken delivery of a large number of Cummins-powered pushboats for their inland fleet. The vessels are sized to share a common versatility with the draft and horsepower to work both the shallower waters of the Intracoastal Waterway and power for the big flows of the

Cummins Vessel Reference #729 S.P. Inter Marine crane barges off loading a cargo ship. Long established in the trucking, warehousing, cargo transfer and barging industry of Thailand, S.P. Inter Marine can be described as a broadly horizontally integrated firm. But established success doesn’t mean they are sitting still. With an well constructed presence at Ayutthaya, about 80 kilometers up the

Cummins Vessel Reference #725 The Sea Cypress completing sea trials.   Over the years, Rodriguez Shipbuilding Inc, of Bayou LaBatre Alabama has probably delivered more shallow-draft tugs than any other US-yard. Their signature lugger-type tug design, with its distinctive aft cabin and wheelhouse, has a strong following amongst US Gulf Coast operators servicing near shore petro-op

Cummins Vessel Reference #726 left to right: Sakchai Rujiphapra, Director, Mahachai Dockyard; Sathit Suwanprasert, Senior Engineer, Marketing Dept., Cummins DKSH (Thailand) and Ku Wee Ming, Manager, Regional Marketing, Cummins Asia Pacific with the newly launched Wonderful Pearl currently being fitted out alongside at the shipyard.   Thailand has long been noted for exquisite fo

Cummins Vessel Reference #724 The Bravante V on sea trials. Long reserved for specialized applications such as icebreakers, diesel electric has enjoyed a rapid growth for marine propulsion in the past decade. Throughout that period, Cummins Marine has been a leader, supplying over 900 diesel electric packages since delivering its first genset 2003. A QSK60 genset ready to delivery from Cu

Cummins Vessel Reference #722 Mr. Ernie: A New Generation in the GOM. The latest delivery from Houma, Louisiana-based New Generation Shipbuilding is representative of the New Generation in supply vessel design. The distinctive bow and focsle profile on the 171 by 36-foot Mr. Ernie is reminiscent of some of the progressive International designs. This can be attributed to additional super structu

Cummins Vessel Reference #720 One of the first steel-hulled crewboats being loaded out in Vietnam. Australia-based Strategic Marine bas built a strong reputation for high performance crew boats. Primarily built at their Singapore shipyard, the aluminum crewboats are available in a variety of sizes and power configurations. In recent years, Strategic has delivered a number of their popular 40

Cummins Vessel Reference #721 The diesel-electric tuna seiner Belle Isle.   As the ex-vessel cost of tuna continues to squeeze the margins for tuna canners, the advantages of high quality and high value sashimi grade tuna become ever more attractive. Writing for their April 2013 in-house publication, SAPMER CEO Yannick Lauri explained the French firm’s Indian Ocean tuna fishery,

Cummins Vessel Reference #719 The 1400 cubic meter capacity LPG tanker ready for delivery. The Saigon Shipbuilding & Marine Industries One Member Co, Ltd. (Saigon Shipmarin) has completed construction of a 60 by 11-meter LPG carrier. With capacity for 1400 cubic meters in two tanks the vessel’s hull has a 4-meter molded depth and a 2.6-meter draft. Designed by a related company to Saigon