AVRA Towage Adds to Fleet | Cummins Inc.
""
Marine

AVRA Towage Adds to Fleet

by Alan Haig-Brown

Cummins Vessel Reference #597

AVRA Towage Adds to Fleet

With the July delivery of the tug Northwind, the Rotterdam-based firm Avra Towage is now operating a fleet of six tugs with a seventh under construction. Three of the Company’s original five-boat fleet have Cummins main engines, so it was an easy choice to go with Cummins engines for the Northwind. However, where the others have 2400 HP and 32 tons of bollard pull with a pair of 38-litre Cummins main engines (tugs South, West, and East), the new boats are powered by a pair of the larger 50-liter Cummins KTA50-M engines. These generate a total of 3200 HP to give the boats bollard pulls of 43 tons.



Full specifications and additional photos for the Northwind, built in Sibu East Malaysia, are available from [email protected].


For further information:

Avra Towage BV
Scheepmakershaven 32b
3011 VB Rotterdam
The Netherlands
Phone: 31 10 281 0886
E-mail: [email protected]

Tan Ju Lin
Commercial Manager Asia
Avra Towage Singapore Pte Ltd.
12A Jalan Samulun
Singapore 629131
Phone: 65 6264 6829

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...