Diesel-Electric Units Prepared for Navy’s AGOR Project | Cummins Inc.
""
Marine

Diesel-Electric Units Prepared for Navy’s AGOR Project

by Alan Haig-Brown

Cummins Vessel Reference #695

A rendering of the AGOR vessels currently underconstruction

 

During most of 2012 Cummins Northwest was busy with the procurement of the various subsystems and assembly of the diesel-electric units for the two Ocean Class Auxiliary General Purpose Oceanographic Research (AGOR) vessels building at Dakota Creek Shipyards They delivered the first four-unit ship set in January of this year. Seattle-based Guido Perla & Associates, Inc has done the design work for the two vessels. Four Cummins QSK38-DM powered electrical generators will provide power for each of these 238 by 50-foot vessels. The generators will provide power to each vessel’s two AC propulsion motors that each turn controllable pitch propellers. Cummins Northwest Inc. has worked with Siemens Industries to develop the generator sets.

 

 

 

One of the Cummins-powered diesel-electric units ready for installation

 

The four gensets on each vessel will also provide power to an azimuthing bow thruster and a tunnel stern thruster as well as general electrical requirements of the vessel. As on the University of Delaware’s 2005-built RV Hugh R. Sharpe, also built by Dakota Creek, the four engines allow for sound reduction when running at slow speeds on only one or two engines as required. 

 

 

 

A stern quarter view.

 

Being built for the US Navy’s Office of Naval Research (ONR), the two vessels, designated AGOR 27 and AGOR 28, are expected to deliver in late 2014 and early 2015. The Woods Hole Oceanographic Institution will manage AGOR 27, while the Scripps Institution of Oceanography will manage AGOR 28 under charter party agreements with ONR.

 

Information released by the ONR explains that: “Both ships will have the ability to sail at a sustained speed of 12 knots and will have 20 berths allotted for crew members and 24 for scientists. Some of the high-tech features planned include: acoustic navigation and tracking systems that operate at various depths; a specially designed hull that diverts bubbles from the acoustic sensor area; a centralized freshwater cooling system to provide heating, ventilation and air conditioning; and dual-controllable propellers with variable speed motors for increased efficiency.

 

 

 

Secretary of the Navy Ray Mabus has announced that, when commissioned, the AGOR 27 will be officially named R/V Neil Armstrong. “Naming this class of ships and this vessel after Neil Armstrong honors the memory of an extraordinary individual, but more importantly, it reminds us all to embrace the challenges of exploration and to never stop discovering,” Mabus said.

 

 

For further information:

 

Joseph Mackes
SEA 05D4
Email: [email protected]
Phone: 202 741 0334

Christopher MacDonald
Email: [email protected]
Phone: 202 781 1158
PEO Ships/PMS325
Assistant Program Manager for AGOR 27/28 POC

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...