Modutech Marine’s Work Boat Medium | Cummins Inc.
""
Marine

Modutech Marine’s Work Boat Medium

by Alan Haig-Brown

Cummins Vessel Reference #827

US Navy Work Boat Medium.

 

The US Navy has some spectacular vessels from submarines to high speed RIBs. They also have dedicated ports and support facilities worldwide. A practical reality of all of this is that the Navy requires efficient and handy boats to support the warhorses. To meet this requirement John Myers of the naval architect firm Hockema & Whalen and Associates have developed a 30 by 15-foot tug with a 5.5-foot draft.

 

 

 

Built at Modutech in Tacoma, Washington

 

Currently the Navy has 24 of these tugs, designated Work Boat Medium, on order from Modutech Marine Inc. of Tacoma, Washington. The first was delivered in December of 2017 with the others to follow in regular deliveries through to December 2019.

 

In order to handle some heavy pushing, the Navy has ordered the vessels to be powered by a pair of Cummins QSL 9 diesels each delivering 285 HP continuous duty. The engines will turn nozzled 39- by 36-inch propellers through ZF W325 gears with 3:1 reduction. Triple shutter-type rudders are mounted behind each prop. The combined 570 HP will give the 30-foot tugs a 17,500-pound bollard pull. Between jobs, the boats will be capable of nine-knot speeds.

 

 

A smart looking and functional craft.

 

Tankage will include a 400-gallon fuel tank. On deck, a 400-pound davit can be moved to port or starboard mounts as required. A pair of Bloom deck winches are mounted forward, port and starboard, so as to function with a pair of cheek blocks mounted alongside the pilothouse for making up to a barge with the push knees. Wide side decks provide a safe work space for the deckhand. A towing bitt is mounted on the after deck. Heavy bollards are mounted on both sides for mooring and for working barges or other equipment on the hip. Lifting pad eyes are built into the tugs’ structure.

 

D-Rubber fendering surrounds the hull, including the chine, and is mounted on the push knees that extend below the waterline. The wheelhouse has overhead windows for working alongside ships. This series of boats have clearly been designed with careful attention to detail and thought to versatility of application and varied roles to which they may be assigned.

Photos courtesy of Modutech

 

For further information:

 

Brian Swindahl
Modutech Marine Inc.
2218 Marine View Drive
Tacoma WA. 98422
Phone: 253 272 9319
E-mail: [email protected]
Web: Modutech Marine Inc.

Mike Fourtner
Commercial Marine Sales
Cummins Northwest
3300 Mottman Rd. SW
Olympia, WA 98512
Phone: 360 748 8841 | Ex 4011
Toll free: 800 451 5506 | Ex 4011
Cell: 360 352 0192
E-mail: [email protected]
Web: www.cummins.com/sales-and-service

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...