Popular Boat: Popular Engine | Cummins Inc.
""
Marine

Popular Boat: Popular Engine

by Alan Haig-Brown

Cummins Vessel Rference #689


On the Mississippi and throughout the US inland waterways pushboats of about 70 feet and with around 2000 hp are ubiquitous. They can be seen in barge fleeting operations along the riverbanks for pushing one or two 30,000-barrel oil barges. In recent years the standard power package has been a pair of Cummins’ popular KV38-M engines. These V-12-clylinder 2300-cubic-inch displacement engines have evolved over the years to take advantage of new technologies and, more recently, to meet new environmental standards.

Gary Eymard has been around the inland towboat world for some time also. His most recent boat is building on spec at his facility on the Ship Canal in Harvey Louisiana. He builds his hulls upside down and then flips them up on the bank beside the canal before putting the fist two levels of deckhouse on. The wheelhouse, for his current 72×30-foot hull will have a 35.5-foot eye level elevation above the water. It will be added later.

With the 7-inch shafts in place before the hull was flipped, he will now add the two Cummins KV38-M main engines with their Twin Disc MGX5321 gears with 5.96:1 ratios. Before launching the 74×58-inch four-blade props will be added. Also added to the Entech and Associates-designed vessel will be the main and flanking rudders.

Calvin Klotz, Vice-President of the Marine Division of Cummins Mid-South reports, “In 2012 we sold a total of 230 of the legendary KV38-M engines to the off-shore and inland river markets. Of these, 170 engines went to 85 push boats. This was a record year for the Tier 2 compliant, 38-liter engine. We look forward to continuing to serve our loyal clients and new customers with our new EPA Tier 3 compliant QSK38-M engines with the recently improved common rail fuel systems.”

When Eymard’s new towboat is ready for delivery in August of 2013 it will have accommodation for a crew of seven in four cabins. Tankage will include 18,100 gallons of fuel, 12,900 gallons of water and 820 gallons of lube oil. In addition to the mains there will be two 65 kW gensets. On deck there will be a pair of Patterson 40-ton barge winches.


Photo courtesy of Eymard Marine Construction and Repair


For further information:

Calvin Klotz
Vice-President
Marine Division
Cummins Mid-South Inc,
110 Airline Hwy.
Kenner, LA 70062
USA
E-mail: [email protected]

Lisa Eymard
Eymard Marine Construction & Repair
2500 Peters Road
Harvey, Louisiana 70058
Office: 504 367 7878
Fax: 504 367 3770
E-Mail: [email protected]

Entech & Associates
761 W. Tunnel Blvd., Ste D,
Houma, LA 70360
Phone: 985 868 5524

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...