Let’s do a fuel comparison: Natural Gas vs Hydrogen | Cummins Inc.

Let’s do a fuel comparison: Natural Gas vs Hydrogen

By Puneet Singh Jhawar, General Manager – Global Spark Ignited Business

scale made of grass

Many commercial fleet operators are thinking about transitioning their vehicles to hydrogen or natural gas engines. These fuels can be great ways to reduce emissions. Both fuel options present similarities and differences across a variety of areas. For example, both hydrogen and natural gas are predominantly used in their gaseous form in vehicle applications. This leads to similarities in some components. On the other hand, there is a huge gap in their availability, resulting in different degrees of adoption.

Natural gas and hydrogen engines: Vehicle hardware comparison

Both natural gas and hydrogen engines are spark-ignited. Many of their components are thus similar, including the engine block, cylinder heads and ignition system.

As is the case with all vehicles, safety is a paramount consideration. Both hydrogen and natural gas vehicles incorporate high-pressure fuel tanks to meet common safety requirements. However, Compressed Natural Gas (CNG) vehicles typically keep natural gas at pressures of around 3,600 psi. Hydrogen vehicles store their fuel at pressures of up to 10,000 psi—that’s higher than the pressure at the bottom of the ocean. Such high pressures are needed because hydrogen molecules contain less energy than natural gas molecules. So, to carry the same amount of energy onboard a vehicle, more hydrogen molecules must be pushed into the same tank, resulting in a higher pressure.

This means that designing and manufacturing safe and lightweight storage tanks for hydrogen vehicles is more difficult. Hydrogen storage is, in fact, a field of thriving innovation.  That’s why Cummins has partnered with NPROXX, a leading innovator and manufacturer of hydrogen tanks. This partnership enhances Cummins’ capabilities in fuel cell and hydrogen production technologies.

Natural gas and hydrogen: what fuel provides the best NOx and greenhouse gas reductions?

Natural gas and green hydrogen are alternative fuels that help reduce emissions in the transportation sector. Replacing a hundred older diesel transit buses with natural gas buses with Cummins’ L9N natural gas engine, would have the same impact as taking 280 gasoline cars off the road. This is substantial, but natural gas vehicles still release CO2 when burning CNG.

Hydrogen vehicles, in contrast, have near-zero tank-to-wheel greenhouse gas emissions, as long as they run on green hydrogen. They can reduce emissions by +99% compared to diesel. You can learn more about how green hydrogen emission reductions compare to different alternative fuels.

Switching to either type of vehicle can also result in lower emissions of air pollutants. Neither generates any soot and no-or very low-amounts of carbon monoxide and organic pollutants. Natural gas engines generate extremely low amounts of NOx. To account for the small traces of NOx tailpipe emissions from hydrogen engines, an aftertreatment system may be needed. Hydrogen Fuel Cell Vehicles, on the other hand, produce no NOx or other air pollutants whatsoever. Hydrogen internal combustion engines and fuel cells have complementary use-cases. Both invest in the hydrogen economy and infrastructure.

Some fleets have already switched to natural gas engines to reduce their GHG emissions by 13-18%. A reduction that can even become carbon negative with renewable natural gas from landfills.

Natural gas and hydrogen: what are some of the infrastructure limitations?

In 2021, there were approximately 1,500 private and public fueling stations offering Compressed Natural Gas, or CNG, in the United States. When comparing CNG to other fuels, it is not as universally available as gasoline and diesel. The CNG distribution network is still far denser than the green hydrogen distribution network though. At the time of publication, there are only 67 public hydrogen fueling stations in the United States, and almost all of them are in California.

The absence of a dense fueling network means that hydrogen is not yet an option for many use cases. In most places, purchasing a hydrogen vehicle is not a feasible option as refueling infrastructure is not widely available. California, Japan, and some parts of Europe are exceptions where hydrogen vehicle ownership is more feasible.

For commercial vehicles, the absence of existing fueling options can be easier to overcome. Businesses interested in switching to hydrogen may have the option to build private hydrogen fueling stations in a central vehicle depot. These stations can be built similarly to CNG, a current practice, or they can place fueling stations along fixed routes between, for example, distribution centers.

Are we moving towards a greater availability of hydrogen?

There is a great deal of interest in the industry around the use of hydrogen engines in medium and heavy-duty applications such as buses and trucks. Other low-carbon alternatives, such as battery electric technology, aren’t always practical for these applications. This is why Cummins is developing hydrogen engines for use in medium and heavy-duty vehicles.

If commercial users adopt hydrogen vehicles, it’s possible that hydrogen fueling stations will become more common. If this is case, then hydrogen vehicles could become a practical option for more users, including potentially private vehicles. This would drive the construction of additional hydrogen fueling stations and attract more users towards hydrogen vehicles. Cummins continues to invest in hydrogen production and electrolyzer technologies.

Battery electric vehicles tend to be more popular than hydrogen vehicles in the personal transportation segment. But there has been an undeniable progress in green hydrogen technology, production capacity, and distribution infrastructure. If green hydrogen continues on that course, availability constraints will be less and less of a factor for fleet operators who are looking to switch their vehicles to an alternative fuel. If you are interested in learning more, don’t forget to check out answers to frequently asked questions around hydrogen engines.

Author Profiles

Puneet Singh Jhawar

Puneet Singh Jhawar, General Manager – Global Spark Ignited Business

Puneet Singh Jhawar is the General Manager of the global natural gas business for Cummins Inc. In this role, he is responsible for the product vision, financial management and overall performance of the natural gas business. Over his 14-year career at Cummins, Jhawar has cultivated successful relationships with a number of Cummins’ largest customers. Jhawar has extensive global experience, with roles based in the Middle East, India, Europe and the US.

Want to find out more?

Receive the latest from Cummins in technologies, products, news, and insights.